cancel
Showing results for 
Search instead for 
Did you mean: 

Does the STM32H750 support multi-drop SWD?

GGonz
Associate

Does the new STM32H750 MCU Family include the ARM CoreSight Serial Wire protocol version 2 in ADIv5.1 released in Sept 2009 which permits support for the multi-drop SWD extensions? The objective being the use of a single SWD debug header to enable debug of multiple MCUs whose SWD are interconnected.

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3

Some of the H7 parts support multiple "Access Ports" via the ST-LINK V3 connection

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Uwe Bonnes
Chief

STM32F7 and STM32H7 supports SWD version 2. So the MCU Idcode is already visible in the in the access port and so it should supports multi drop. Probably L5 will also be protocol version 2. Let's see.

Khouloud GARSI
ST Employee

Hi @GGonz​ ,

Indeed, the STM32H750 supports Serial Wire Debug protocol version 2, which provides a multi-drop capability.

Khouloud.