2018-04-13 10:52 PM
Hi,
I am trying to learn PWM generation with STM32F030F3P6. Generated code using STM32CubeMX. Basic PWM generation worked fine.
Now I am trying to change PWM pulse width dynamically in while loop of
main(). Please see my main function. I am trying to fade-in and fade-led. But LED remains turned-off.
int main(void)
{
uint16_t pwm_value = 0;
uint16_t step = 10;
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_TIM14_Init();
HAL_TIM_PWM_Start(&htim14, TIM_CHANNEL_1);
while (1)
{
HAL_Delay(100);
if(pwm_value = 0) {
step = 50;
}
if(pwm_value >= 1000) {
step = -50;
}
pwm_value += step;
__HAL_TIM_SET_COMPARE(&htim14, TIM_CHANNEL_1, pwm_value);
}
}
�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
Here is full main.c file (most of comments are stripped out).
#include 'main.h'
#include 'stm32f0xx_hal.h'
TIM_HandleTypeDef htim14;
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_TIM14_Init(void);
void HAL_TIM_MspPostInit(TIM_HandleTypeDef *htim);
int main(void)
{
uint16_t pwm_value = 0;
uint16_t step = 10;
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_TIM14_Init();
HAL_TIM_PWM_Start(&htim14, TIM_CHANNEL_1);
while (1)
{
HAL_Delay(100);
if(pwm_value = 0) {
step = 50;
}
if(pwm_value >= 1000) {
step = -50;
}
pwm_value += step;
__HAL_TIM_SET_COMPARE(&htim14, TIM_CHANNEL_1, pwm_value);
}
}
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct;
RCC_ClkInitTypeDef RCC_ClkInitStruct;
/**Initializes the CPU, AHB and APB busses clocks
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
/**Initializes the CPU, AHB and APB busses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSE;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
/**Configure the Systick interrupt time
*/
HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);
/**Configure the Systick
*/
HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);
/* SysTick_IRQn interrupt configuration */
HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);
}
/* TIM14 init function */
static void MX_TIM14_Init(void)
{
TIM_OC_InitTypeDef sConfigOC;
htimInstance = TIM14;
htimInit.Prescaler = 7;
htimInit.CounterMode = TIM_COUNTERMODE_UP;
htimInit.Period = 1000;
htimInit.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htimInit.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
if (HAL_TIM_Base_Init(&htim14) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
if (HAL_TIM_PWM_Init(&htim14) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
sConfigOC.OCMode = TIM_OCMODE_PWM1;
sConfigOC.Pulse = 0;
sConfigOC.OCPolarity = TIM_OCPOLARITY_LOW;
sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
if (HAL_TIM_PWM_ConfigChannel(&htim14, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
HAL_TIM_MspPostInit(&htim14);
}
/** Configure pins as
* Analog
* Input
* Output
* EVENT_OUT
* EXTI
*/
static void MX_GPIO_Init(void)
{
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOF_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
}
void _Error_Handler(char *file, int line)
{
while(1)
{
}
}
�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
PWM generation woks good if I remove code lines within while loop and put any desired value for line:
sConfigOC.Pulse = 0;�?
As far as I think, I am not calling __HAL_TIM_SET_COMPARE() right way or something else is required there. Could you please help me to identify that?
Thanks in advance. #stm32-f0 #timer #pwm2018-04-15 3:10 AM
Fill in all fields of sConfigOC.
JW
2018-04-15 9:24 AM
Consider using a scope to check the signal.
Consider using a lower frequency so you can perceive the on/off time.
Try a fixed 50/50 duty at 1Hz
2018-04-15 11:49 AM
MX_TIM14_Init() already contains setting up with all required fields filled in. Remaining parameters are OCIdleState and OCNIdleState, those are only valid for TIM1 and TIM8 (as per HAL code documentation comments), while I am using TIM14.
2018-04-15 11:59 AM
... and OCNPolarity but you are right, those you've set appear to be sufficient.
Read out and check/post the content of relevant GPIO and TIM registers.
JW
2019-02-05 11:36 PM
if(pwm_value = 0) {
step = 50;
}There is a misstake in your main. You use a assignment operator "=" instead a comparison operator "==".
The rest should work;)