STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Using an STM32F031, can I have one ADC channel being monitored by analog watchdog and another channel being scanned in each iteration of the main loop?

Lets say I have channels 1 and 2.I was wondering if I disable continuous scan and enable watchdog on 2. Will the interrupt for channel 2 be called only when I do a start scan or will the watchdog keep continuously checking the channel 2?In other word...

SSudh.12 by Associate
  • 589 Views
  • 0 replies
  • 0 kudos

STM32 Rotary Encoder Pulse Count

Is it proper way to to count encoder pulses using rising/falling edge interrupt instead of using Timer in Encoder Mode??Because in my application I need interrupt above 80000 pulse count. But here timer is of 16-bit (STM32F103C8T6) so it can only cou...

JPanc.1 by Associate II
  • 1289 Views
  • 1 replies
  • 0 kudos

STM32F030C8 warm start failure

We have several STM32f030C8s that refuse to start if the ambient temperature is 40deg C. Below, say 20 deg C, they start and continue to run up to and beyond 40 deg c ok. Applying a reset on a stalled processor brings it to life. Is this a known p...

DPidd by Associate II
  • 2291 Views
  • 5 replies
  • 0 kudos

Resolved! Rotary Encoder Application

I am using STM32F103C8T6 for counting rotary encoder pulse.My Encoder PPR is 5000.But when I program for timer1 as encoder mode and show count on segment it shows 20000 pulse per rotation it is 4 times higher than the actual value. What should I do t...

JPanc.1 by Associate II
  • 2125 Views
  • 3 replies
  • 0 kudos

How to do STEP/DIR interface?

Hello,I need to connect STEP/DIR driver (DRV8825 to STM32F103) for driving one axis stepper motor. I will use buttons for moving and I need to set acceleration and deceleration profile. Do you have some experience what way of pulse generation I shoud...