User Activity

Posted on January 10, 2018 at 02:34HiAN4861 (http://www.st.com/content/ccc/resource/technical/document/application_note/group0/25/ca/f9/b4/ae/fc/4e/1e/DM00287603/files/DM00287603.pdf/jcr:content/translations/en.DM00287603.pdf) page 25 states that th...
Posted on January 09, 2018 at 07:07We are designing for an application having front and back-facing 7' displays.  I am keen to hear suggestions for running both displays from the same processor using using LTDC or display peripheral?Both displays wi...
Posted on March 31, 2014 at 21:32I am receiving this compiler error in SystemNDrivePrarms.h on lines 8182, 8216, and 8250 when compiling MCTasks.c.  (MC version: 3.4.1, IDE: IAR EW for ARM 7.10)  ID_DEMAG,        /*!< Demagnetization current in s16A...
Posted on March 28, 2014 at 11:35Hi I am running the Motor Control library 3.4.1 on the STM32F107xC. It keeps crashing into the 'Hardware Fault' exception. I have made the necessary adjustments to the IAR project build, and had to adjust some define...
Posted on March 25, 2014 at 01:02Hi The motor control SDK 3.4 provides me with an LCDProject, which I believe contains the binary for the communications interface to the Motor Control Workbench program. There doesn't seem to be any source code provi...
Kudos from