STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Error in the reference manual?

Hello,I would like to signal a possible error on the reference manual of the STM32L496 (RM0351 Rev 6)At pag 348, section 11.4.5, Table 45 the first line (source port 8bit, destination port 8bit) indicates that the Number of data items to transfer is ...

ADC DMA not work

HelloWe ran the ADC DMA on the HAL example source. However, I tried to write the source in CUBEMX, When executed, the DMA interrupt is executed once and is not executed again.Please let me know if I missed anything

HG LEE by Associate II
  • 1249 Views
  • 1 replies
  • 0 kudos

STM32H743 Internal voltage Reference and the ADC.

I am using the STM32H743II package (with Vref+ and Vref-). Those two pins are not connected in this design (they're left floating). I'd like to measure the temperature of the chip, and am having trouble using the internal voltage reference as the ref...

jgroff by Associate
  • 2394 Views
  • 2 replies
  • 0 kudos

STM32L Discovery, How to output HSI with MCO

Hello.I am currently developing with STM32L Discovery.In preparation for development, I tried to output using the MCO in order to know the exact frequency of the HSI of the evaluation board used.By operating MCOSEL in the RCC-> CFGR register, MSI and...

ota-s by Associate II
  • 6518 Views
  • 10 replies
  • 0 kudos

DMA memory to peripheral question.

Hello,I have a doubt regarding DMA memory to peripheral ?Suppose I would like to transfer a memory buffer content to SPIx TX.When do each transfer occurs ? Every time I change the content of the memory buffer ? Always ?I cannot find this information...

simo zz by Senior II
  • 1394 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.