STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Need help understanding performance issue on STM32H743

I'm struggling to understand why I'm seeing a huge performance hit by slightly changing code in a loop. I narrowed down the problem to a manageable code size, and I'm hoping someone here can suggest how to investigate and resolve my issue.I'm using a...

fbar by Senior
  • 3979 Views
  • 5 replies
  • 0 kudos

Used SPI 4 for two different interfaces

Hi All,I am using STM32F427ZIT6 MCU for one project. I connected SPI4 for two different interfaces by mistake. Pins 1,4,5 for one interface and pins 64,65,66,67 for one interface.I want both the devices working simultaneously. Is there any solution f...

DKS by Associate II
  • 1137 Views
  • 1 replies
  • 0 kudos
DBroo.1 by Associate III
  • 1430 Views
  • 3 replies
  • 0 kudos

SD Card Time out STM32F779II

I'm using STM32F779II With a microsd card. That is clocked at 48MHz.When writing to the sdcard as a block, I get HAL_TimeOut, using that function: err = HAL_SD_WriteBlocks(&sd_handle, (uint8_t *)src, block_num, num_blocks, 6000);After writing I wait ...

Receiving a burts of data from SPI using DMA

Hi, I am using an STM32f407VGT MCU and I am trying to receive a burst of data of 112 bytes from SPI1 and storing it in an array buffer, initially set with all its elements to 0.According to the RM0090 TRF this should be easily done with the DMA, but ...

simo zz by Senior II
  • 3614 Views
  • 12 replies
  • 0 kudos

Linker Error: "no definition for __write".....

Hey everyone, I am using IAR and a STM32F401RE.When I am setting the library low-level interface implementation to "None", I get the following linker error:Error[Li005]: no definition for "__write" [referenced from fflush.o(dl7M_tlf.a)]Error[Li005]: ...

JCorn.2 by Associate II
  • 4653 Views
  • 2 replies
  • 0 kudos

Resolved! I have a question about using flash memory.

HI Sir.I will try to work on a project using STM32.I have a question regarding flash memory usage.I want to  save input data to flash memory but STM flash memory is divided sector.The capacity of each sector is determined.ex) STM32F205VE Sector 0 : 1...

User.72 by Associate II
  • 1531 Views
  • 2 replies
  • 0 kudos

H743vit SDMMC2 not working

hii want to have both SDMMC 1 and 2 i test my project for SDMMC1 in 4bit sdio at 44MHz and no clock Div its work good singlebut when i set SDMMC2 single with that not worki change setting reduce frequency , use clock div , software pull up pins but ...

stive by Associate II
  • 5321 Views
  • 14 replies
  • 0 kudos