cancel
Showing results for 
Search instead for 
Did you mean: 

What are the required voltage levels for the OSC-IN pin for the HSE clock when using an external crystal resonator.

JEsko
Associate II

I see that if using an external CMOS oscillator on just the OSC-IN pin that 0.3*VDD and 0.7VDD input levels or better are required. My external crystal oscillator using OSC-IN and OSC-OUT has a smaller voltage swing than 0.3VDD to 0.7VDD. Do the same levels apply in both cases? ST app note for oscillator design provides many other guidelines but not voltage levels.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
T J
Lead

usually its a small sine wave

this one H743,

is 0.3V peak to peak centered at 1.6V

8.0003MHz