I start the safety functional software by the example from "STM32CubeExpansion_STL_G0_V1.1.0".
From the readme.txt, it mention "Install ST CRC tool", but it is "STM32CubeProgrammer", is this tool has built in CRC function? by post-build steps command...
I'm using TrueStudio for my previous product coding/debugging. I downloaded some example projects from ST website, there are options for IAR/Keil/STM32CubeIDE, is TrueStudio fully replaced by STM32CubeIDE?I'm get used to TrueStudio, is STM32CubeIDE...
Try to use STM32G0 LQFP32 MCU do accuracy frequency measurement, but there is no HSE crystal interface, so internal HSI RC will be for system clock, the accuracy of the system clock will affect the frequency, how accuracy is internal HSI RC clock
STM32 MCU has 12 bits ADC resolution, but some MCU claim "up to 16-bit with hardware oversampling". When I setup ADC in STMCubeMX, no option for "hardware oversampling", how to achieve 16-bit ADC resolution?
We have two "P-NUCLEO-LRWAN1" bought several years ago, it is obsolete from ST,I try to play with LoRa, is "I-CUBE-LRWAN" still can work with those kit?
When I was using TrueStudio, it seems better than Eclipse for debugging, the product is already in the market, just add some new feature if required, I will keep TrueStudio for it. My new design will use STM32CubeIDE for coding/debugging.
Hi Piranha,It's nice to hear your experience, this is what exactly I want to know. Two questions:You setup the A/D setting manually or by STMCube? 256X oversampling, that means sampling 256 times for each conversion, that will slow down the sample ra...