STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F407 external interrupt PD11 not working

Hello,I'm using the Pins PC0, PD11 and PD12 in my application as external interrupts with rising edge. To handle the interrupt, I'm using the functions EXTI0_IRQHandler() for PC0 and EXTI15_10_IRQHandler() for PD11 and PD12. In both functions is the ...

user 143 by Associate III
  • 1806 Views
  • 3 replies
  • 0 kudos

F407 Hard Fault

Hello,I am woking with CMSIS RTOS v1 on STM32F407 mcu,and every time after ~30 mins my device gets haurd fault.void vListInsertEnd( List_t * const pxList, ListItem_t * const pxNewListItem ) { ListItem_t * const pxIndex = pxList->pxIndex; // <------- ...

0690X00000ArsXKQAZ.png
qqAnton by Senior
  • 2378 Views
  • 4 replies
  • 0 kudos

HELP !! FMC what is going on

Hello any help appreciatedtrying to work out out how the FMC peripheral works on the STM32F767ZI armwould like to interface an FPGA to the 767 arm as an external memory device using a multiplexed Address & Data Bus, but so little info on the FMC out ...

0690X00000Arrz3QAB.jpg 0690X00000Arrz8QAB.jpg 0690X00000ArryoQAB.jpg 0690X00000ArrzDQAR.jpg
JHERI by Senior
  • 3084 Views
  • 9 replies
  • 0 kudos

Use systick as a timer and read timer value

i am new in stm32 . i am using stm32lo31 series nucleo board . i want to read push button press timing so i am using polling method to detect read button press event. then i want time between press event to release. how can i configure systick to...

problem with stm32f103c8t6

Hi guy, i'm new to stm32. I'm using stm32f103c8t6, my problem is that when i upload the code with stlink, and without switching boot0 back to 0, my program work fine, but when i reset by reset button or power this board with usb cable, it doesnt work...

Understanding CAN external loopback mode

Hello,STM32H7 contains example for  CAN external loopback mode.In the readme there is no mention for the need of wiring a physical loopback between tx and rx pins.Is it required in the external loopback mode ?Thanks

ranran by Senior II
  • 9203 Views
  • 9 replies
  • 0 kudos

Resolved! Target not created

Hello,i build the code of "STM32F4DIS-BB Software Examples 20130307: STM32F4xx_Camera_Example" but it can't create the .axf file. who had an idea?Thanks.

0690X00000ArrslQAB.png 0690X00000ArrsgQAB.png 0690X00000ArrsbQAB.png 0690X00000ArrsRQAR.png
MHMallek by Associate II
  • 3987 Views
  • 4 replies
  • 0 kudos