User Activity

Hello.I was developing a GUI with STM32F767 & RGB TFT LCD.However, the specification has changed and I should consider changing to the STM32H743.Are there any issues to watch out for when changing the cpu?Does CubeIDE & TouchGFX Deginer support H7 de...
H​ello.I am trying to make a touchgfx demo using stm32f767 apollo board.However, I was stuck while applying a custom external loader using w25q256.I've modified the code from my existing 746-disco demo and it doesn't work at all.Dose anyone have exam...
How can I check the revision of the m7 core without checking the registers?The revision r0p0 and r0p1 have a problem. When debugging  jump to a timer interrupt or debug sequence is bad.So I would like to know how to check revision in advance when buy...
Hi.I am using the uart on the touchgfx project on the stm32f746-disco board, but when I continue the uart interrupts, I get stuck.There were two cases of stuck state.1. Screen stops but uart is running2. Board is completely frozenThe uart interrupt c...
When I run the program like the picture below, a checksum error occurs.After that, if I reset the hardware, it will work normally.I guess it is a problem caused by using external memory.But I want to know the exact reason why and I want to fix it.Ple...
Kudos given to