STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H750xB errata 2.2.18 cannot be reproduced. "DAC GPIO cannot be used when DAC is connected to on-chip peripheral only"

I would like more information regarding errata 2.2.18 for STM32H750VB Silicon Rev V, from document DM00399555, which reads:"When a DAC output is connected only to an on-chip peripheral, the corresponding GPIO is expected to be available as an output ...

0690X00000BvuMaQAJ.png
RMart.0 by Associate III
  • 2915 Views
  • 7 replies
  • 0 kudos

UARTs receive buffer in STM32F030

Hi all,I'm trying to use a example which works and compile correctly on stm32f103 (cortex-m3) family.Now i want to use this example on stm32f030c8t6 ,but there is erorr on line 6:BOOL xFCPortSerialGetByte( CHAR * pucByte ) { /* Return the byte in t...

Resolved! I ran the following code to reconfigure the SPI running on an STM32F103, but the DMA settings do not seem to be updated. Is there any solution?

// SPI_HandleTypeDef *hspi // DMA_HandleTypeDef *hdmatx   hspi->Init.DataSize = SPI_DATASIZE_16BIT; hdmatx->Init.MemInc = DMA_MINC_DISABLE; hdmatx->Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD; hdmatx->Init.PeriphDataAlignment = DMA_PDATAALIGN_HAL...

Takeshi by Associate II
  • 1711 Views
  • 4 replies
  • 0 kudos

Data Buffer for serial and spi

hi hope have good dayi need to buffer data for save on every 1ms for serial and spi i use dma to receive datafor example hal_uart_receviveDMA on this function must set buffer size ...i test one example :50Hz send to mcu data each time 1000 and 1001 ...

MacLaren by Associate III
  • 4433 Views
  • 10 replies
  • 0 kudos

STM32H743 runs in debug mode only

Hi, I have several boards with same issue. After weeks of tests when flashing boards using STLink suddenly the micro is not running except in SWD debug mode. Flash is properly programmed but the micro is not running. A complete flash erase (all sec...

DGall by Associate II
  • 2684 Views
  • 3 replies
  • 0 kudos

Error working with stm32f030?

In a project I need to use an eeprom, I download st-s eeprom library for stm32f0xx ( AN4061 ). The provided example in keil mdk v4 had no errors however after I imported the eeprom.h and .c file in my own project in keil mdk v5 I started having probl...

AJava.5 by Associate
  • 875 Views
  • 0 replies
  • 0 kudos

STM32F030C8 I2C1 in BUS_BUSY after first start pulse.

First I thouht that problem in code generation from Cube, rewrote all in CMSIS, but nothing changed. I2C using only as a "slave", but after generation "start" and sending addres (0x70) + write no interrupt flags is set. Where my mistake?Initialisatio...

Wanderer by Associate
  • 854 Views
  • 1 replies
  • 0 kudos