STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

RTC on B-L475E-IOT01A.

At evening I set time 18-38-00, got it back, it was OK and left it to run. At morning I see the time 32-59-48. My set-get functionsint RTC_SetTime(uint8_t hours, uint8_t minutes, uint8_t seconds) { if (hours < 24 && minutes < 60 && seconds < ...

Dear all, I am working on FDCAN with STM32G473 and I do not understand the example calculation of the Baudrate in chapter 43.4.7 in the following document RM0440 Rev 2 (en.DM00355726.pdf)

bit time = [NTSEG1 + NTSEG2 + 3] tqAnd in the note With a CAN kernel clock of 48 MHz, the reset value of 0x06000A03 configures the FDCANfor a bit rate of 171 kbit/s.NSJW = 6NBRP = 0 => 1NTSEG1 = 10NTSEG2 = 3How do you get 171 kbit/s by 48 MHzBest Reg...

HUnso.1 by Associate
  • 685 Views
  • 0 replies
  • 0 kudos

Which communication should I use if I want to transmit 2.6 MSPS sampled signal to PC using STM32H743ZI ?

Hi I am currently developing a radar backend system wherein I need to pass ADC sampled data at 2.6 MSPS to PC for post processing. I am stuck to which communication type will be optimal for transmiting such data from STM32H743ZI to PC.

NKarn.1 by Associate II
  • 1043 Views
  • 2 replies
  • 1 kudos

I am using STM32F407vg, i wrote a code for ADC while debugging value is not updating no errors as well in the code. i connected a 10K potentiometer to PA0, i checked with DMM no issues. I am adding my code snippet please let me know the mistake.

/* Includes ------------------------------------------------------------------*/ #include "main.h" #include "stm32f4xx_rcc.h" #include "stm32f4xx_gpio.h" #include "stm32f4xx_adc.h"   /* Private variables ----------------------------------------------...

psati by Associate II
  • 1179 Views
  • 1 replies
  • 0 kudos

reset timer count value

i wrote a program and i want to turn on the led after passing a 500 and 750 , 1000ms.i use out put compare and use active on mach timer mode.but it only work one time , i realize that i should reset my timer and count value but i don't know how?plea...

Aes.1 by Associate
  • 1225 Views
  • 1 replies
  • 0 kudos