User Activity

HiI have been working with the Nucleo F401RE + P-NUCLEO-53L0A1 sampling the VL53L0X, and it was working fine. However interfacing the Nucleo F401RE  to another VL53L0X module (https://picclick.de/VL53L0X-Time-of-Flight-Distance-Sensor-Breakout-GY-VL5...
HeyWe are using the STBC08 to charger a LiPo battery, the device charges to 4.2v which is the maximum voltage for battery, However I understand that charging to 100% is not optimal in terms of battery lifetime, and most sources recommend not charging...
I am try to connecting a STM32 Nucleo (F401RE) to a ESP8266 on UART.I've managed to control the ESP8266 with the PC using a usb/uart channel and hyperterminal.I've managed to send uart messages to the PC from the NucleoBut I am unable to command the ...
VL53l0X / i2c problemTrying to use I2C to read vl53l0x, I fail to understand from the datasheet :1. what exactly are the indexes and what indexes I'm suppose to use when reading,2. Also how many bytes include in one data sample ?From the data sheet I...