STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Import a projet to a different evaluation card

Hello,I am currently working on a project integrating the ST package (fp-aud-smartmic1) allowing to test acoustic improvement functions (echo cancellation, beamforming ...) however I wish to work on a different microcontroller than the one proposed i...

UTANG.1 by Associate II
  • 1264 Views
  • 3 replies
  • 0 kudos

Switch Block influencing stop2?

I'm seeing the following problem:In normal Mode, the current function to run, is from a swich/case block inside main();. This works perfectly fine in run mode. Some cases end up in STOP2, and change state (the switch/case) variable after the wakeup p...

STM32L010RB, STOPmode with RTC wakeup.

New to STM32 low power devices.I cannot get power consumption of the nucelo to below 120ua when measuring at IDD. I have configured the ISR and RTC as per NUCLEO-L031K6\Examples\PWR\PWR_STOP_RTCAny assistance would be highly appreciated. I can get th...

UART IT not working on STM32L0K8T6

Hey guys, i'm back.I'm trying to configure UART on STM32L0K8T6. The goal is just to send data to this MCU via TeraTerm and send data from MCU to PC.To do so, i used CUBEmx to easily configure UART but the fact is I can send data from MCU to PC but S...

0693W000000UqVaQAK.png
AJT by Associate III
  • 1985 Views
  • 4 replies
  • 0 kudos

stm32F4 and CAN bus

hi there,i am working on a project and i have to connect two stm32F4 boards via CAN bus. i ve been looking on the internet for days now but i can't manage to find a circuit nor a code to that. i desprately need your help. thank u.

SGUIG.1 by Associate II
  • 674 Views
  • 0 replies
  • 0 kudos

Details on STM32G474 DMAMUX?

The information in the reference manual (RM0440) is very limited. There is an app note: "AN5224 DMAMUX description" but it says it only covers STM32H7, STM32G0, STM32L4+ and STM32WB series.Also, if you search the resources for the STM32G474 this appl...