STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L412C8 USART2 RX TX pin swap not working

I am using the STM32L412C8 and I am having trouble with the USART2 RX/TX pin swapping. I enabled it in CubeMX but if I send data to the PA2 pin (originally TX but should be RX after the swap) I get nothing. If however I send my data to PA3(should be ...

KAsim by Associate II
  • 7145 Views
  • 17 replies
  • 0 kudos

It seems that using the comparators with interrupts on the stm32f373 series with HAL drivers blocks the program in infinite loop.

I attach the full code as a file and the relevant part here - for the evaluation board STM32373C-EVAL in which the red LED blinks a few times until the comparator is activated and blocks the execution.Is there a workaround to make the comparator work...

Empty check flag on STM32F030 (option bytes)

Hello,I have a problem when flashing my MCU (STM32F030CCT).After flashing, a Power On reset is always needed to start my SW (to reload the option bytes due to the "empty check flag").From manual: On STM32F070x6 and STM32F030xC devices only, internal ...

Stabilo by Associate III
  • 2497 Views
  • 3 replies
  • 0 kudos

STM32L4Px characteristics on the WWW page are false

On the page :https://www.st.com/content/st_com/en/products/microcontrollers-microprocessors/stm32-32-bit-arm-cortex-mcus/stm32-ultra-low-power-mcus/stm32l4-plus-series/stm32l4p5-q5.html?querycriteria=productId=LN2188$$1=STM32L4P5#then product selecto...

ADC self calibration, needed or not ?

Hello,I have a project where my ADC channels will be calibrated end of line using a calibration bench. I will directly calibrate the physical measurements (voltage and current). My question is: do I need to implement the ADC self-calibration sequence...

Stabilo by Associate III
  • 1507 Views
  • 2 replies
  • 0 kudos

Resolved! How to set ADC SOC at half of duty cycle Ton?

Hi,I'm designing a power supply using a stm32F334R8 Nucleo board. For the application is interesting to trigger the ADC SOC at half the Ton (In order to measure average current).I am using STM32CubeIde. I have read the reference manual and the HRTIM ...

0690X00000DXHrtQAH.png
mur by Associate III
  • 1219 Views
  • 1 replies
  • 0 kudos

Why FMC bus turnaround time is so long in mode D on STM32F303?

I'm using STM32F303ZE MCU's FMC(FSMC) to communicate with a special chip. FMC is cofigured in NOR/PSRAM mode, asynchronous, non multiplexed, timing mode D (see attached FMC configuration in CubeMX). FMC clock is equal to AHB MCU clock that is 70MHz. ...

0693W000000Uo8AQAS.jpg
RGris by Associate II
  • 3357 Views
  • 4 replies
  • 0 kudos