STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Fast correlation slower than regular?

Arm_correlate_fast_q31 takes almost twice as much time as arm_correlate_q31.Am i missing something? I measured the calculating time for arm_correlate_q31 for various block sizes and then simply inserted the "fast_" in the function call and it takes a...

RMcCa by Senior II
  • 1231 Views
  • 1 replies
  • 0 kudos

Hardware bug STM32F11 in Timer DMA mode (PWM Generation)

I wanted to generate PWM Waveforms with nucleo F411and found a severe bug in the hardware. Maybe it is described in the errata sheet, but I found nothing.bug:DMA is dependent on data send on DMA stream. Sometimes DMA transfer is not done. (DMA circul...

rzong.1 by Associate II
  • 2444 Views
  • 9 replies
  • 0 kudos

Resolved! How to receive stream through SPI using DMA ?

Hi, I am using an STM32F407VGx MCU and I am trying to receive data from SPI1 using DMA.STM32CubeIDE generated code for the SPI1 is the following:void MX_SPI1_Init(void) { LL_SPI_InitTypeDef SPI_InitStruct = {0};   LL_GPIO_InitTypeDef GPIO_InitStr...

simo zz by Senior II
  • 2076 Views
  • 1 replies
  • 0 kudos

STM32 NUCLEO-F746ZG HSE on-board oscillator from X3 crystal

HiI use STM32 NUCLEO-F746ZG development board for my project. I split the ST-LINK and target STM32 part (Cut PCB). I tried to use HSE on-board oscillator from X3 crystal. I soldered the NX3225GD-8.000MEXS00ACG04874 8-MHz crystal oscillator and two 4....

0693W000000V2xCQAS.png
Onur1 by Associate
  • 2195 Views
  • 3 replies
  • 0 kudos

STM32L412C8 USART2 RX TX pin swap not working

I am using the STM32L412C8 and I am having trouble with the USART2 RX/TX pin swapping. I enabled it in CubeMX but if I send data to the PA2 pin (originally TX but should be RX after the swap) I get nothing. If however I send my data to PA3(should be ...

KAsim by Associate II
  • 7064 Views
  • 17 replies
  • 0 kudos

It seems that using the comparators with interrupts on the stm32f373 series with HAL drivers blocks the program in infinite loop.

I attach the full code as a file and the relevant part here - for the evaluation board STM32373C-EVAL in which the red LED blinks a few times until the comparator is activated and blocks the execution.Is there a workaround to make the comparator work...

Empty check flag on STM32F030 (option bytes)

Hello,I have a problem when flashing my MCU (STM32F030CCT).After flashing, a Power On reset is always needed to start my SW (to reload the option bytes due to the "empty check flag").From manual: On STM32F070x6 and STM32F030xC devices only, internal ...

Stabilo by Associate III
  • 2461 Views
  • 3 replies
  • 0 kudos

STM32L4Px characteristics on the WWW page are false

On the page :https://www.st.com/content/st_com/en/products/microcontrollers-microprocessors/stm32-32-bit-arm-cortex-mcus/stm32-ultra-low-power-mcus/stm32l4-plus-series/stm32l4p5-q5.html?querycriteria=productId=LN2188$$1=STM32L4P5#then product selecto...