STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! what if PA2=5V in analog mode?

I can c in RM0033 (Rev9) Figure 18, that PA2 is connected with low impedance to a diode to V_DD, if PA2 is configured as analog input...In Doc ID 15818 Rev 9 I see that R_ADC is at least 1.5kR...If I connect PA2 in analog mode directly to 5V: Would I...

RRIDDICC by Associate III
  • 1424 Views
  • 4 replies
  • 3 kudos

Resolved! VDD12DSI pins in STM32H747BIT6

Hello everyone,I am working on a system based on the STM32H747BIT6 MCU and do not plan to use the DSI interface. I have searched through various forums but still have some doubts about the proper power pin configuration when DSI is not in use. Here i...

Resolved! can't connect to STM32F407IGT6 on custom board

I have a custom board based on the STM32F407IGT6 and I'm having trouble connecting via ST-Link (v2 clone) using STM32CubeProgrammer. It seems st-link unable to find the target mcu. I checked all SWDIO, SWCLK, NRST, VDD, GND connections with a multime...

Screenshot from 2025-05-24 15-43-53.png schematics.jpeg
tskn by Associate
  • 1406 Views
  • 3 replies
  • 0 kudos

How to sample improve ADC speed?

My application senario: sample the sensor signal every second, and transmit through UART. to save power supply, I select ADC single mode, and used average as filter.void ConfigureADC(void) { ADC1->CFGR1 |= ADC_CFGR1_AUTOFF; ADC1->CFGR2 = (ADC1->CFGR2...

STM32L09 by Associate II
  • 2688 Views
  • 8 replies
  • 3 kudos

Interrupt Vector Table

Hello,As per CM4 guide and TRM of Nucleo f446re,interruot vector table is array of function pointers and each pointer holds the entry address(initial address) of each IRQ_handler, Where interrupt IRQ_number is used for indexing.While debugging I fail...

Screenshot 2025-05-14 222309.png Screenshot 2025-05-14 222359.png Screenshot 2025-05-14 222411.png

UART RX DMA Implementation Issue

Hello,I am using STM32F030C8T6 to implement Modbus RTU protocol which uses UART and RS485 as physical layer.I have already implemented the complete protocol with UART's RXNE and TCIE interrupts.Now I am trying to implement through DMA by which I will...

Anesh by Associate III
  • 1948 Views
  • 0 replies
  • 0 kudos