STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32G4 HRTIM burst mode enable / disable

In the reference manual for the G474, under HRTIM Burst mode control register (HRTIM_BMCR), bit 31 is the BMSTAT register; it gives the current operating status of the burst mode feature. But it states that writing this bit to zero causes early burst...

Jbin0101 by Associate III
  • 1601 Views
  • 1 replies
  • 0 kudos

SPI Slave on STM32G030F6 is not working

Hi, This is my first time here to write a post. I want to implement a system that connnects a STM32H723(master) and four STM32G030F6P6s(slave) via SPI communication. I connected  them and I check the SPI signals from STM32H723(NSS, SCK, MOSI). The Si...

JCho.3 by Associate III
  • 1694 Views
  • 3 replies
  • 2 kudos

STM32F103 Bootloader Fails to Jump to Application

Hi everyone,I'm new to bootloader development and currently working on my first STM32 bootloader project using an STM32F103. I’m trying to make a minimal bootloader that simply jumps to an application located at 0x08001000. There’s no USB, no UART, n...

FMAC implementation

Hi allI have an IIR filter design with 7 coefficients. (For feed-forward and for feed-back)Regularly all the coeffs are between -1 to +1So I Just multiply each by 2^15 to get it in q1.15 format.However, now, the feedforward coeffs are very small (0.0...

yonatan by Associate III
  • 2188 Views
  • 6 replies
  • 1 kudos

Resolved! STM32F205RG USB High Speed and I2C RTC Problem

Greetings,In my application i have initialized STM32F205RG with USB High Speed Host for detecting USB Key board and I2C2 for communicating with DS3231 RTC Module. RTC module works prefectly when i don't initialize USB HS peripheral, but when both ini...

Resolved! what if PA2=5V in analog mode?

I can c in RM0033 (Rev9) Figure 18, that PA2 is connected with low impedance to a diode to V_DD, if PA2 is configured as analog input...In Doc ID 15818 Rev 9 I see that R_ADC is at least 1.5kR...If I connect PA2 in analog mode directly to 5V: Would I...

RRIDDICC by Associate III
  • 1405 Views
  • 4 replies
  • 3 kudos