STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-NUCLEO-IDB05A1 fireware update field!

Hi, I is developing a BLE appilication using X-NUCLEO-IDB05A1 module. I use FlashUpdaterTool (Version 2.1.0) to connent my NUCLEO board of L476RG (VirtualCOMPort Application V0.0.1 ), which connect X-NUCLEO-IDB05A1 module. During updating the fire...

0693W000000WXfzQAG.png
xqiu.1 by Associate
  • 715 Views
  • 0 replies
  • 0 kudos

RTC second advanced and SSR greater than PREDIVS

Hi,​I​ am using stm32f779 RTC upto subseconds granularity that is using SSR register value for giving upto milliseconds level of time output .The scenario is such that there is external time source ( network clock) to which I synchronise RTC by updat...

A Maq by Senior
  • 1603 Views
  • 3 replies
  • 0 kudos

DMA Problem with USART

Hello,I have written these codes for transmitting an array to USART.1)The Message[21] Array fills up every 200us. It sets Flag=1 when data is ready.2) If the user makes the PB11 pin low it starts DMA section to transmit the data.(All data will transm...

parisa by Senior
  • 1223 Views
  • 1 replies
  • 0 kudos

Resolved! Starting timers in one pulse mode

Hello everyone,I read many of the posts on the forum and couldn't find an answer to this question: is there any way to start timers in one pulse mode other than through an external stimulus? that is, only through software? How could it be done?I am l...

LCatL by Associate II
  • 3497 Views
  • 2 replies
  • 1 kudos

STM32L4xx reference manuals System clock (SYSCLK) selection

RM0351 and RM0392 (and maybe others, haven't checked them all) contain this in the System clock (SYSCLK) selection sectionStatus bits in the Internal clock sources calibration register (RCC_ICSCR) indicate which clock(s) is (are) ready and which cloc...

berendi by Principal
  • 1508 Views
  • 2 replies
  • 1 kudos

Resolved! STM32F429I-EVAL Board FW

Hi -I have a STM32429I-EVAL board. Before I start mucking about with it, I would like the original firmware file (bin or hex file). I may want to go back to the original demo fw at some point. Here is the system info:Demo Rev: 1.4.5Board: STM324x...

Mary West by Associate II
  • 2106 Views
  • 3 replies
  • 0 kudos

Resolved! STM32H75O-DK Demo - does it run from RAM or QSPI?

Hi folks​I​'d like to ask about STM32H750B-DK. This a demo board based on the Value Line STM32H75O with 128kB Flash and 1 MB RAMI saw its demo​ movie on the YouTube and would like to understand whether it runs from the Flash or RAM? Or in other word...

Yevpator by Associate III
  • 2326 Views
  • 3 replies
  • 0 kudos

Resolved! How to use JTAG interface instead of SWO on a NUCLEO-144?

Hi everyone!I'm pretty new with STM32 microcontroller and STM environment. Now I'm playing with a Nucleo-H745ZI board and developing using STM32CubeIDE. This board is equipped with the st-link V3. It should be able to use both SWO and JTAG interface ...

Gabriele1 by Associate II
  • 4263 Views
  • 4 replies
  • 0 kudos