STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to stabilize and increase camera frame rate?

Hello, I've recently took over a project at my school where they are building a wearable camera. They have used STM32L496ZG as the MCU. Basically there are two sensors on the board: OV2640 and MLX90640. One takes regular JPEG and the other takes ther...

ESaat.1 by Associate
  • 1811 Views
  • 1 replies
  • 0 kudos

How to achieve 8nA in shutdown mode with wakup pin on L412?

Hello,I'm experimenting with ulp I'm starting from lowest power consumption achievable and add peripherals and wake up conditions to see what happens.That's why I'm starting with shutdown mode. I'm using a custom board with only an STM32L412K8, few c...

JulienD by Senior
  • 2077 Views
  • 6 replies
  • 0 kudos

Resolved! HAL_FLASH_Program not writing to flash permanently

Hi all,I am using HAL_FLASH_Program() to program an uuid into a specific address. I can verify it write successfully by reading from the address. However, if I power cycle the MCU, the memory at that address returns to the original value. If I write ...

vtran1 by Associate II
  • 9329 Views
  • 18 replies
  • 0 kudos

NUCLEO-G071RB compatible to which Expansion Boards?

Hello together,I'm totally new to the STM32 world, so sorry in advance for the stupid question.I just bought a NUCLEO-G071RB and would like to combine it with some Nucleo Expansion Boards. Is every Nucleo Expansion Board compatible with my Controller...

FSchm.1 by Associate
  • 657 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.