STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Multiple read from Peripheral to Memory using DMA

Dear Experts,Can I configure the DMA2 to do say 3 repeats read on GPIOx_IDR by a single DMA request? I do not want to have array of bytes instead I would like to write into a single variable and overriding it with the latest value.I have set the MINC...

ADC whit DMA. stm32f0

Hi every one.I want to read the value of a potentiometer connected to the pinA1, and if the read value is more than 2000, one of the LEDs, otherwise the second LED, will be on.Can anybody please help me? what is wrong with my code? I don't have too m...

Nmo.1 by Associate III
  • 2391 Views
  • 5 replies
  • 1 kudos

STM32f4 Timer1 counting pulses

Hello all, I want to count pulses with TIMER 1, because he has the fastest counting frequency. I was able to count pulses with TIMER 2 but something in my code is missing to make it work for Timer 1: (I also checked the reference manual ...)Maybe som...

MKell.2 by Associate II
  • 3844 Views
  • 8 replies
  • 0 kudos

Resolved! STOP2 mode scrambles stack on STM32L4R9

I'm really struggling with this problem. This is my first time trying to do anything low power, so please forgive any noob mistakes. All I'm trying to do is get the hang of a simple low power program so I can apply it to a larger one. My code is here...

CBald by Associate III
  • 2378 Views
  • 2 replies
  • 0 kudos

STM32F105 flash programming through CAN

I have an application where I must be able to update the code remotely through the CAN2 link and the embedded bootloader. This worked fine using the mass erase function, but now I need to erase sectors individually. The ap note AN3154 poorly describe...

JBizo.1 by Associate
  • 1893 Views
  • 3 replies
  • 0 kudos

Bare metal STM32F767 PCB design

Hello This is my first time using STM32 MCU on my own PCB. I know that I have to take many things into consideration. Please help me if I am missing somethingI have wired up all VDD/VSS/VDDA/VSSA/VUSB with bypass caps as close as I couldI have used e...

hashtala by Associate II
  • 2055 Views
  • 6 replies
  • 0 kudos

Resolved! ADC power circuit

Hello, I am developing a circuit using STM32L4R9AI, VDD = 1.8v, VDDA&VREF+ = 3.13v, according to ST hardware design manual (I attached) for a better power filtration there should be bead between VDD and VDDA, will that create a problem given the volt...

STm32L496 IAP and BLE

Hi !I've been trying to update my STM32L496 firmware over BLE.Our bootloader use Ymodem to transfer files (as it's explained in the Application note). I have connected the UART of my BLE chip with the UART of the STM32). I can send the file (only fro...

FGuil by Associate
  • 1440 Views
  • 1 replies
  • 1 kudos

Resolved! ADC overrun error. Multiple DMA usage.

Hi,I am using a NUCLEO F334 development board.I am using the ADC with the DMA. I developed that feature and tested and everything looked alright. I have been developing some more over that and I see that after startup the values are correct but after...

0693W000000WxBRQA0.png 0693W000000WxBHQA0.png
mur by Associate III
  • 9783 Views
  • 10 replies
  • 0 kudos