STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Can't program STM32F301K8U7

I can't download rom file when using STM32F301K8U7.The programmer can connect the MCU and recognize it. But there always are errors when modifying the flash. All reading data are 0xFF, even after I erasing the total chip.The programmer I tested are ...

LW.2 by Associate
  • 1118 Views
  • 0 replies
  • 0 kudos

STM32 timer3

Hi everyone. I wrote this code to run the stm32f0 timer3, which toggle 2 LEDs at a time, but it doesn't work. Can anyone please help me؟void TIM3_Init() { TIM_TimeBaseInitTypeDef TIM3_InitStructure; NVIC_InitTypeDef NVIC_InitStructure;   ...

Nmo.1 by Associate III
  • 1197 Views
  • 2 replies
  • 0 kudos

Nextion Communication issue

HelloI have Nextion display. Ican control it with arduino library in Arduino ide good.I am learning communication nextion without itead nextion library via uart.I designed simply page in nextion. it has just a textbox named "t0".I try send a word fro...

0693W000001qeRtQAI.png
FLine.1 by Associate II
  • 2713 Views
  • 4 replies
  • 0 kudos

BSP_AUDIO_OUT_Play works only when the data pointer is external flash in memory mapped mode. STM32H747HI-DISCO

Hello,I would really appreciate a hint to understand why BSP_AUDIO_OUT_Play works if the data pointer is external flash memory in memory mapped mode. But doesn't work when the data pointer is a global array in RAM.When it does't work with RAM pointer...

ALevc.1 by Associate III
  • 1687 Views
  • 2 replies
  • 0 kudos

A very quick question regarding creating a new project.

My Windows desktop computer has failed so I'm trying to get all happening on a MacBook Pro.When a project is created I'm supposed to get a message box asking me if I want to "initialize all components in their default mode." That way all the clock, ...

JMazu.1 by Associate III
  • 2176 Views
  • 3 replies
  • 0 kudos

STM32 UART Interrupt between 2 STM32F103C8 boards.

Hello guys good day. I would like to ask for your suggestions regarding the UART interrupt between 2 STM32F103C8 MCUs. I can transmit and receive between 2 MCUs using a single input and output with the use of the IRQHandler. However when I wanted ...

RSy.1 by Associate III
  • 2956 Views
  • 8 replies
  • 0 kudos

Resolved! stm 32F4 Virtual comport won't work

Hello,i am trying to use the virtual comport of the stm32f407vgt6 to communicate with my win 10 pc. I want to send 16 bytes of data. I created a base project in cubeMX and insert the cdc_transmit. There it is possible to send 16 bytes of data via the...

FD.1 by Associate II
  • 2484 Views
  • 2 replies
  • 0 kudos

I have a strange phenomenon in stm32f103

HelloI have a hw configuration that uses mpu6050, lora chip, gps, and bluetooth using stm32f103 mcu. I use lithium polymer 3.7v 1300mah for power to board.It doesn't make sense to me, but it's like this.After downloading the firmware via stlink, mpu6...

Jlim.1 by Associate II
  • 3852 Views
  • 13 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.