STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

arm_sqrt_f32 and arm_math.h

Hi, I'm using Cube and Makefile.I'd like a clearer run through of how to make use of the sqrt f32 function in arm_math.h.. The header doco says to copy the header to Include, done.. Then link the Lib for big/little endian. Here's where I'm stuck, how...

d4 by Associate III
  • 5820 Views
  • 8 replies
  • 0 kudos

We are using HAL library for F215xx and F746xx MCUs. We found difference for CAN driver within HAL_CAN_GetRxMessage() function for setting the RTR (remote transmission request) register. Are more detailed information about sFIFOMailBox availalbe?

stm32f2xx HAL library version 1.8.0 & 1.9.0pHeader->RTR = (CAN_RI0R_RTR & hcan->Instance->sFIFOMailBox[RxFifo].RIR);stm32f7xx HAL library version 1.14.0 & 1.15.0pHeader->RTR = (CAN_RI0R_RTR & hcan->Instance->sFIFOMailBox[RxFifo].RIR) >> CAN_RI0R_RTR_...

PDell by Associate
  • 800 Views
  • 0 replies
  • 0 kudos

HI, I programmed F103RB with SW4STM32 as following. LED is blinking as expected but I have Following Confusions/Questions. In Status Register flags for OCx for all channels are set however chanels are not enabled.

#include "stm32f10x.h"#include "stm32f10x_rcc.h"#include "stm32f10x_gpio.h"#include "stm32f10x_tim.h"int main(void){GPIO_InitTypeDef GPIO_InitStructure;GPIO_StructInit(&GPIO_InitStructure);RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE);GPIO_Ini...

WRaso.1 by Associate II
  • 2150 Views
  • 4 replies
  • 0 kudos

STM32G4xx process technology (nm)

Hello,I would like to know the process size used in the STM32G4xx. I understand the 'F4, L4 and G0 are 90 nm and the 'H7 is 40nm. My interest stems from an application in a high RF environment, where larger process size would seem to be more robust...

Resolved! Failing to receive data on MCU set up as SPI slave

Trying to receive data on MCU (L432KC) configured as SPI slave. I have tried using interrupt and DMA, but no luck. I have set up the circuit like this : 1 MCU acts as master sending 1,2,3 every 500ms interval (I hooked up master lines to scope and th...

0693W000001rE5UQAU.png 0693W000001rE5PQAU.png
KSchr.11 by Associate II
  • 5245 Views
  • 12 replies
  • 0 kudos

Tracking an optical encoder overflow and underflow

I'm using an STM32F407 MCU with a 600 PPR incremental optical encoder. The encoder is coupled to a stepper motor that drives a 5mm pitch ballscrew. I'm trying to keep track of the encoder count to determine the absolute position of the spindle attach...

Is dual bank flash configuration available for STM32H743xxxx?

In STM32F7 dual/single bank configuration is available. It can be done using nDBANK bit of FLASH_OPTCR register. Ref link: https://www.st.com/resource/en/application_note/dm00266999-stm32f7-series-flash-memory-dual-bank-mode-stmicroelectronics.pdfFor...

VViro.1 by Associate
  • 3133 Views
  • 4 replies
  • 1 kudos

CMSIS examples for stm32

Hello guys.Eventually I have to learn how to use CMSIS my self to create my own code instead of using CUBE.There was alot of examples for everything in CUBE,but I cant find examples written in CMSIS.Can someone help me finding them?The other question...