cancel
Showing results for 
Search instead for 
Did you mean: 

UART RX FIFO not working

ROost.1
Associate

I can’t seem to get the FIFO to work on the RX side. TX works fine.

Seems as if the FIFO isn't used. If I interrupt on the "RX not empty" event and read the data, it works fine. But as soon as I want to interrupt on any FIFO event, I never get the interrupt.

When I manually read the receive side of the UART, there really is just one byte in there. Almost as if there is no FIFO on the RX side.

huart8.Instance = UART8;

huart8.Init.BaudRate = 115200;

huart8.Init.WordLength = UART_WORDLENGTH_8B;

huart8.Init.StopBits = UART_STOPBITS_1;

huart8.Init.Parity = UART_PARITY_NONE;

huart8.Init.Mode = UART_MODE_TX_RX;

huart8.Init.HwFlowCtl = UART_HWCONTROL_NONE;

huart8.Init.OverSampling = UART_OVERSAMPLING_16;

huart8.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;

huart8.Init.ClockPrescaler = UART_PRESCALER_DIV1;

huart8.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;

HAL_UART_Init(&huart8);

HAL_UARTEx_EnableFifoMode(&huart8);

SET_BIT(huart8.Instance->CR1, USART_CR1_RXFFIE);

...

void UART8_IRQHandler(void)

{

  uint32_t isrflags  = READ_REG(huart8.Instance->ISR);

  if (isrflags & USART_ISR_RXFF)

  {

     ....

  }

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
turboscrew
Senior III

Which devices are you talking about? In most STM32s, there are no UART FIFOs. DMA is used instead.