2020-02-14 3:56 AM
Hello,
I am trying to figure out how long an ADC in dual mode and DMA will run to take 24000 samples. I cannot get any proper values.
My init at startup:
bitset(SCB->ConfigCtrl, bit9); // set STKALIGN in NVIC
bitset(SCB->AIRCR, (0x5FA<<16)|(3<<8)); // init Priority, 4 Bit Pre-Emption, 4 Bit Subpriority
bitset(FLASH->ACR, 0x12); // Flash 1 wait state
bitout(RCC->CFGR, bit16); // HSE oscillator clock selected as PLL input clock (8MHz)
bitset(RCC->CFGR, (0b0111<<18)); // PLL input clock x 9 (72 MHz HCLK)
bitout(RCC->CR,0x01010082); // enable ext. high frequency OSC and PLL, bit 16: HSE ON, Bit 24: PLL ON
while(bittst(RCC->CR, bit17)); // wait until the HSE is ready
while((RCC->CR & (1<<25)) == 0); // wait until the PLL is ready
bitset(RCC->CFGR, bit1); // PLL selected as system clock
while ((RCC->CFGR & 0x0C) != (2<<2)); // wait till SYSCLK is stabilized
bitset(RCC->CFGR, (0b100<<8)); // APB low-speed prescaler (APB1) HCLK divided by 2
bitset(RCC->CFGR, (0b000<<11)); // APB high-speed prescaler (APB2) HCLK divided by 1
bitset(RCC->CFGR, (0b10<<14)); // ADCPRE /6So the ADC clock should be running at 12 MHz. Is this correct? Crystal is 8 MHz. I checked this with the config tool of the CubeIDE (which I am not using for the project). bitset simply does an x | value and bit out does a x = value.
So then I initialize the ADC and DMA before a sample:
bitset(RCC->AHBENR, bit0); //enable DMA clock
bitset(RCC->APB2ENR, bit9); //enable ADC1 clock
bitset(RCC->APB2ENR, bit10); //enable ADC2 clock
bitout(ADC1->CR1, 0);
bitout(ADC1->CR2, 0);
bitout(ADC2->CR1, 0);
bitout(ADC2->CR2, 0);
bitout(DMA1_Channel1->CCR, 0);
bitout(DMA1->IFCR, 0xFFFF);
bitset(ADC1->CR1, bit18|bit17|bit8); //regular simultaneous mode
bitset(ADC2->CR1, bit18|bit17|bit8);
bitset(ADC1->CR2, bit20|0b111<<17|bit1); //SWSTART, continuous
bitset(ADC2->CR2, bit20|0b111<<17|bit1);
bitset(ADC1->CR2, bit8); //set DMA for dual ode
bitset(DMA1_Channel1->CCR, 0b11<<12); //set DMA1 channel priority to very high
bitset(DMA1_Channel1->CCR, 0b10<<10); //set memory size to 32bit
bitset(DMA1_Channel1->CCR, 0b10<<8); //set peripheral size to 32bit
bitset(DMA1_Channel1->CCR, bit7|bit3|bit1); //enable DMA1 memory increment mode and interrupt (for flags)
bitset(DMA1_Channel1->CNDTR, buffer_size); //set amount of reads to size of data buffer (can be changed later)
bitset(DMA1_Channel1->CPAR, (uint32_t)&ADC1->DR); //set peripheral address of DMA1 channel1 to ADC1 data register
bitset(DMA1_Channel1->CMAR, (uint32_t)&data_adc); //set memory address of DMA1 channel1 to location of data buffer
bitset(DMA1_Channel1->CCR, bit0);
vectors_set_priority(11, 15, 15);
vectors_enable_interrupt(11);
bitout(ADC1->SQR1, 0); //one channel
bitout(ADC2->SQR1, 0);
bitout(ADC1->SQR3, 14); //ADC1 channel 14 PC4
bitout(ADC2->SQR3, 15); //ADC2 channel 15 PC5
if(adc_sample_time > 7) adc_sample_time &= 0b111;
bitout(ADC1->SMPR1, adc_sample_time<<12); //sampletime
bitout(ADC2->SMPR1, adc_sample_time<<15);
bitset(ADC1->CR2, bit0);
bitset(ADC2->CR2, bit0);
bitset(ADC1->CR2, bit3); //reset calibration
bitset(ADC2->CR2, bit3);
while(bittst(ADC1->CR2, bit3)); //wait for calibration reset
while(bittst(ADC2->CR2, bit3));
bitset(ADC1->CR2, bit2); //start calibration
bitset(ADC2->CR2, bit2);
while(bittst(ADC1->CR2, bit2)); //wait for calibration
while(bittst(ADC2->CR2, bit2));
bitset(ADC1->CR1, 0b0110<<16); //ADC1 and ADC2 in dual modebuffer_size is 24000, adc_sample_time is 0 at first.
So my question is, how do I calculate the time of one sample (and thus the total time) for the all the values of SMP 0 to 7 in the ADC_SMPR1?
It seems 1/12 MHz * the SMP value (1.5, 7.5, 13.5 etc) is not the solution. In the ref.man. it says one conversion at 72 MHz takes 1.17 µs. But how is this connected to the SMP in ADC_SMPR1?
Edit: I foud out about the 12 cycles + SMP. The values still dont match up. It seems the time is of by a factor of 2 as if the ADC clock was 24 MHz... Otherwise its ok.
:weary_face:
Thanks