Hi, just want to know if it is possible to switch the interrupt between Character match and Each character received interrupt on the fly without stopping the UART ?
Hi, I have the below code where I trigger the UART DMA and write to a buffer, and in the while loop I simply do a read from the buffer 1st element:MX_UART7_Init();
Uartret = HAL_UART_Receive_DMA(&huart7, uartbuf, 300);
while(1){
if(Uartr...
Is there a way to stop STM32 PWM after 10 pluses ?I know one solution is using the system time and issue a stop via the code, however my issue is the stm CPU might be very busy to handle the stop signal.