Skip to main content
Martin Izaak
Associate II
February 29, 2020
Question

STM32F0 and SPI with CPHA=1 an NSS pin

Hello Forum,

I am new to STM32 but familiar with MCUs. My Problem is the SPI interface.

In the datasheet there is a figure (figure 277 of document RM0091) where all four possible combination of CPOL/CPHA are shown. There is also the signal nss in the figure.

I can reproduce all settings except CPHA=1 where the NSS signal disappears. On other place in the data sheet there is written that NSSP=1 is not possible if CPHA=1. SSOE did not work as I expect but that is an other topic... NSSP switches the NSS signal on/off.

My DAC needs a CS (NSS signal) and a pause between two samples and also CPOL=1/CPHA=1.

So is there a way to set CPOL=1 and CPHA=1 and have also a valid NSS signal on the GPIO pin?

Thank you for your help!

Martin

This topic has been closed for replies.

5 replies

KnarfB
Super User
February 29, 2020

You can use a GPIO for SS which you toggle by software. That is some overhead, but it works.

Martin Izaak
Associate II
March 1, 2020

Thanks for the hint. I am not used to solve things by software, which work perfectly in hardware elsewhere.

Or is the software work around the only way to solve this?

Martin

KnarfB
Super User
March 1, 2020

> Or is the software work around the only way to solve this?

Unfortunately, yes.

Martin Izaak
Associate II
March 5, 2020

OK, I will to this GPIO workaround. This will reduce my DAC update rate by a factor 4, but I will not deal with additional NSS overhead...

waclawek.jan
Super User
March 5, 2020

For periodic transfers, if only one SPI frame per transfer is needed, one possible solution would be to use a timer - one channel would generate the SS/framing signal, other would trigger a DMA transfer from memory into SPI's data register.

JW