STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB OTG HS bandwidth

Hi everyone,I'm developing a USB OTG Highspeed using STM32F756ZG with USB3340 USB PHY.Currently I'm using two OUT endpoint (EP1 and EP2), the host PC send each request (EP1 --> EP2 --> EP1 --> EP2 and so on). I got a problem when I try to send a requ...

anhdv_0-1748919233891.png
anhdv by Associate
  • 870 Views
  • 1 replies
  • 0 kudos

Resolved! Floating ADC value even when pin is connected

Hello !I have to admit that I am stumped on this problem, I've been trying to make it work for the past few days.My issue is with an STM32F301K8T6 (LQFP32) and its ADCs : I have two reflective optical sensors (ITR8307) that are connected to ADC_CHANN...

Whitebow by Associate II
  • 4405 Views
  • 10 replies
  • 1 kudos

Resolved! Wakeup pin hardware design specs?

Hi! I am working on a project in which I'd like to use an stm32U0 MCU. It'll be my first time with one of these, and I'm choosing it because my design includes a battery (+charger & fuel gauge), so I'm interested in learning about low-power things. I...

sb_st by Senior II
  • 1114 Views
  • 2 replies
  • 3 kudos

Resolved! Needed LPTIMER valid reinitialize sequence

Hello,I have problem statement, in which I have to re-Initialize lptimer for different timer value, as per current scenario, I haveClock: 32Khz (LSI)Divisor = 128Period: Any time as per dynamic input. So I want information about how I can safely rese...

HYPERBUS

I am using the OCTSPI1 of STM32L4Q5CGTX to set HYPERRAM to memory-mapped mode.Memory can be read and written correctly.When I use STM32CubeIDE to check the HYPERBUS signals with an oscilloscope while the CPU is stopped with a break during program exe...

K_I by Associate II
  • 897 Views
  • 2 replies
  • 0 kudos