STM32G4 USART - Busy Flag and Timeout operation
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2025-01-17 7:16 AM
How does the (USART_ISR) BUSY flag get reset? The data sheet indicates "end of reception," but that is not defined. Is it an end-of-frame, idle event, or something else?
Labels:
- Labels:
-
STM32G4 Series
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2025-01-17 9:08 AM
Hello @2jjayne ,
This bit indicates that the RX line is active and receiving data when it is set, and it gets cleared by hardware at end of reception (stop bit detection) or in case of unsuccessful reception due to halting or other errors, so it can have many conditions clearing it in case of unsuccessful reception.
Regards
In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.