STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Timer for generating 1us tick

I'm using STM32F108RG on 48MHz clock configuration.I need to generate a 1 micrososeconds timer tick on it, for driving an output pin interfaced with a 3rd party device. Using PWM is not an option available.I tried configuring TIM3 with following para...

SShid by Associate III
  • 8369 Views
  • 10 replies
  • 0 kudos

stm32 IAP Binary problem

I am getting this error while debugging "Break at address "0x20004000" with no debug information available, or outside of program code". I am attaching main and linker file. How to solve this? Thanks in advance..

STM32L0 ADC voltage calculations

I have been trying to calculate voltage of the battery connected to ADC_IN7 of STM32L010K8. I have connected a battery to it via voltage divider. When I read the ADC I get raw values of 1948 for applied voltage of 3.7V. After going through the datash...

ARai by Associate II
  • 3915 Views
  • 4 replies
  • 0 kudos

Resolved! STM32L475VG DAC configuration issue: no signal observable on GPIO?

I'm trying to get a very simple example working with the DAC on the STM32L475VG in the B-L475E-IOT01A development board. I've generated the code below with STM32CubeMX for use in STM32CubeIDE. I can see the DAC register values changing, and LD1 blink...

BHM by Associate II
  • 2969 Views
  • 5 replies
  • 0 kudos

SPI DMA Stream Seems to Eventually Freeze

Hi,I'm using CubeMX generated HAL drivers to use SPI in DMA mode. In my particular situation, we are sending a small amount of data (3 bytes) very often over the SPI interface. The data transmission works fine most of the time, but sometimes (as litt...

Drew M by Associate II
  • 2267 Views
  • 4 replies
  • 0 kudos

Hello everyone, I am using stm32f207zg with usb ttl converter with ftdi chip. I want use the usart1 for communication with PA9 e PA10 pins as TX and RX of usart1. I use as virtual terminal, termite, and when i play the program, appear weird characters.

#define RCC_CFGR *((long*)0x40023808)#define RCC_CR *((long*)0x40023800)#define RCC_AHB1ENR *((long*)0x40023830)#define GPIOC_ODR *((long*)0x40020814)#define GPIOA_MODER *((long*)0x40020000)#define GPIOA_OTYPER *((long*)0x40020004)#define GPIOA_AFRL ...

FCa.1 by Associate II
  • 4026 Views
  • 11 replies
  • 0 kudos

Why can not change DBGMCU->CR in STM32F103

I'm use STM32F103C8T6. I use DBGMCU->CR = DBGMCU_CR_TRACE_IOEN to change the value of DBGMCU->CR, but the operation is failed after POR, the register is alway read 0.I suspect that the cause of this problem is the the debug component is not be powere...

Bpan.1 by Associate
  • 2041 Views
  • 3 replies
  • 0 kudos