STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

RTC in Hardware Layout

I am going to use RTC in my application to generate time stamps. I am currently using Nucelo - L412KB evaluation module. Do I need to connect any pins or add any components? Where can I find this information?

Anonymous by Associate II
  • 1691 Views
  • 2 replies
  • 0 kudos

SPI output is wrong

I have STM32F407 that is communicating with TFT lcd over SPI. What I am seeing with Logic Analyzer doesnt match what I am sending. I cant see the pattern, but data is consistent, so its probably some setting that is off. I tried all combinations of C...

Gossamer by Associate II
  • 1266 Views
  • 5 replies
  • 0 kudos

Problem with Flash_Write after a reset

Hi,I'm using the FLASH_Write function in order to save a table in a specific address. Once it is saved correctly I reset the board and try to change another address with the same function.The problem is that the flash_write function works at the firs...

Moughit by Associate III
  • 2291 Views
  • 2 replies
  • 0 kudos

I2C SDA abnormal

When I used the STM32L412KB as an I2C slave. when there only one slave on the bus, all the function works well. but if there hastwo devices on the bus and continue to access one slave device, the non-addressed I2C slave will damage the SDA bus. I cap...

Haifeng by Associate II
  • 2635 Views
  • 3 replies
  • 0 kudos

CAN error 0x000E0000

Hi, I have STM32F091RC board and I am using CAN interface to read CAN BUS data from car. CAN works when I am powering STM32 from USB port (U5V). When I try to power STM32 from car (with E5V port), I get error in can interface 0x000E0000.What could be...

JBond.1 by Senior II
  • 780 Views
  • 0 replies
  • 0 kudos

Calling multiple time __HAL_UART_GET_FLAG in UART

When I try to print on the serial interface with SerialPrint function.  void SerialPrint(const char *serial_data, ...)   {     char uartbuffer[1024];   va_list arg;   va_start(arg, serial_data);   uint16_t len = vsnprintf(uartbuffe...

DCtech by Associate II
  • 2413 Views
  • 1 replies
  • 0 kudos

Resolved! Creating a "Delay by x microseconds" function using TIM6

Hi, I'm trying to understand what I'm doing wrong that the following function seems to delay by anywhere between 667ns and 5.67us even though it's being called as Delay_us(4)I'm using Nucleo STM32F446REvoid KJO_TIM6_Init(uint16_t arel) { LL_APB1_GRP...

kj.obara by Associate III
  • 5882 Views
  • 11 replies
  • 0 kudos

PGSERR and PGPERR Problem

I have a problem with PGSERR and PGPERR bits being set after reset operationI am using stm32f4 board than I am using CANBUS and FW update process.When I use serial debug print in MX_CAN1_Init function. I faced with flash erasing error. Then I analyse...

DCtech by Associate II
  • 3100 Views
  • 7 replies
  • 0 kudos