User Activity

I want to implement Control flow monitoring in application software as mentioned in STM32G0 Series safety manual (UM2455) Page 13 (CPU_SM_1).Can you please provide some example or reference how to implement the same?Thanks
Hi everyone,I am trying to implement SRAM Parity bit check in my application. But when I am enabling it from option byte. and then it is going into Hardfault whenever I am going into debug mode before running application even it is going into .Hardfa...
Hi everyone, We are developing safety device which need to go in a fail safe mode in any kind of failure to achieve SIL2 or SIL3 level of safety. And we want achieve UL certification.And we are using STM32G0B1CBTx MCU. And for writing code I am refer...
We are using STM32G0B1CBT MCU in our product. We assembled 10 pieces and out of 10, 2 devices are randomly going in hard fault sometime instantly after reset and sometime even after 1 hour. What would be the cause? What measures should be taken to re...
I am using stm32f7.When I am using fsdata_custom.c from example file then everything is working perfect. Means Web page is opening on web browser and when I am sending GET request from postman software then MCU is responding with 200 OK. But when I a...
Kudos from