STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

RM0316 ('F303) typos

1) Index contains SYSCFG_MEMRMP but there's no such register in 'F3032) in 5 figures' caption, AUTODLY is mentioned, but there's no such bit, the correct name is AUTDLY (without "O", bit 14 of ADCx_CFGR).JW

Resolved! Performance characteristics of SDRAM on STM32F7508-DISCO board

Below is my benchmarking of multply-accumulate performance on contiguous memory blocks on the STM32F7508-DK board for three different types of memory (on-chip SRAM, external SDRAM managed by the FMC, and QSPI-connected NOR flash):The horizontal axes ...

0693W000002lEueQAE.png
GSpre.1 by Associate III
  • 5456 Views
  • 5 replies
  • 2 kudos

HAL_I2C_Mem_Write() is not setting the address Write bit

I am using the HAL library on a STM32L476RG and have been having trouble getting data out of a sensor. By looking at the signal with a scope I've noticed that the write bit of the device address is not being set when I try to write to the sensor's re...

CGrov.1 by Associate II
  • 1639 Views
  • 1 replies
  • 0 kudos

I2C data always 0x00

I have an stm32L476RG and am trying to read data from a digital magnetometer (MMC5983MA). The I2C connection is working, and I am able to read the slave ID and the slave status. However, whenever I try to read data, it always returns 0x00 for all thr...

CGrov.1 by Associate II
  • 3270 Views
  • 4 replies
  • 0 kudos