Stack aligment in STM32f103, bit STKALIGN
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-04-27 1:59 AM
HI. I'm trying to understand what is Stack aligment and what is it for.
Cortex-M3 has a special bit STKALIGN in SCB->CCR register. Theoretically this bit is set to 1 in new revision of core, but when i look through debugger this bit is clear.
I've read that there is a sepcial attribute for GCC ARM :
__attribute__((interrupt))
and it should be used with old revision r0p0 to align the stack by compiler, but when i make the code i do not know what is the revision of core in uC so do i need to use this attribute or not?
And what happen when do not make aligment?
Labels:
- Labels:
-
STM32F1 Series
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0