cancel
Showing results for 
Search instead for 
Did you mean: 

32L0538Discovery ADC

MNguy.3
Associate

Hello,

When trying to use ADC, I ran into a problem that I don't really understand.

If I try to use ADC through the PA4 pin, the values read fine and are correct.

However, when I try to use any of the other pins for ADC, none of them seem to read the correct values.

Any help / explanation as to why this may be happening would be appreciated.

Thank you.

Edit:

I've also tried the code on two other 32L04538Discovery boards and the same problem persists. PA4 works fine for ADC, but none of the other pins do.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
waclawek.jan
Super User

Are the pins you've tried disconnected from the on-board circuitry of the 'L053DISCO board?

JW