STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

32F051K86 GPIO initialization problem LL_ libraries

I have a bootloader + 1 wire serial uploader codebecause of space restrictions it uses LL_ libraries for initialization.We have different hardware designs, when using PA2 as IO pin it works !when using PB4 as IO it does not !The main program uses HAL...

Adrian.M by Associate II
  • 2026 Views
  • 5 replies
  • 0 kudos

Setting up DMA for UART on the H745 M4 Chip

I'm trying to setup a GPS sensor (UBlox Max8Q) with a H745 Nucleo board using UART DMA using STM32CubeIDE. However, I’m having problems with setting up my board properly. My plan is to eventually do all my data acquisition on the M4 chip and do compu...

How can I search for MCUs that support ETM or ETB?

We are evaluating the use of ETM or ETB but have problems finding MCUs that support those features (or one of them). Sure we can dig into the data sheet of an MCU family but isn't there a possibility to filter for these features in some MCU finder?

FS.1 by Associate III
  • 1013 Views
  • 2 replies
  • 0 kudos

Resolved! MCU doesnt wake up from standby with WKUP1 pin

Hello,I am using STM32L073V8T .I am trying wake up from standby with WKUP1 pin. It is PA0. According to techinical documents, low to high transition should wake MCU from standby. But, It doesnt work in my case. Is there any special configuration what...

CYesi.1 by Associate II
  • 3164 Views
  • 3 replies
  • 0 kudos

pointer typecasting

As per image sub=7(not typecasted), sub1=28(typecasted). I don't understand why is sub giving wrong value I understand I have not typecasted but,each pointer variable is holding 4 byte value (i.e int type) then,typecasting must not be required isnt i...

0693W000003QfNyQAK.png
Disha by Associate II
  • 928 Views
  • 1 replies
  • 0 kudos

STM32F429 program failed, chip locked?

Hi everyone,I built a custom board with STM32F429VIT with the following settings:Boot0=GND, Boot1=GNDHSE=25MHzI configured IAR project options as following:- use-Flash-loader checked;I am using IAR 8.10 with ST-Link-v2 (SWD) to develop the firmware. ...

0693W000003QeLeQAK.jpg 0693W000003QeSYQA0.png 0693W000003QeSsQAK.png 0693W000003QeTWQA0.jpg
ZRong.1 by Associate
  • 1683 Views
  • 0 replies
  • 0 kudos

DMA UART with HAL remains busy bug new version

I generated the code for the uart in dma mode in a cube. But the data does not go, and the HAL_UART_Transmit_DMA function returns HAL_BUSY.I already found a solution to the problem, just publish it.The cube generates code: MX_USART2_UART_Init (); MX_...

IK.2 by Associate
  • 757 Views
  • 0 replies
  • 0 kudos

Hello group. I'm working on a project with stm32-f412zg mcu board and having some trouble in configuring multiple timers using FreeRTOS for stm32-f412zg to control ws2812b led strips. I really need help in implementing it to complete the project. Any help

We are using WS2812b LEDs for output signals. We are able to configure multiple timers simultaneously but the colors are not what we trying to give signal to the WS2812b LEDs. With individual LEDs everything is fine and we are controlling it as we wa...

KVinc.2 by Associate
  • 644 Views
  • 0 replies
  • 0 kudos