STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! SRAM2 parity checking.

I am using an STM32L452CE. I copy an executable (.bin) from Flash to SRAM2. I zero out the remaining SRAM2. I then 'jump' to the executable now in SRAM2. When I have the parity error checking off (FLASH_OPTR_SRAM2_PE = 1) it works fine. When I turn i...

GFalz.1 by Associate
  • 1682 Views
  • 3 replies
  • 0 kudos

Resolved! Where can I find a list of register names for ST32?

I recently changed the chip i'm using for a project. I'm trying to port code between an STM32F031K6 and an STM32L412K8 but some of the registers seems to be called different things. In particular any reference toADC1->CHSELR doesn't work. Where can I...

deep_rune by Associate III
  • 1763 Views
  • 4 replies
  • 0 kudos

Using I2S on IT with STM32F407, I observe that the SPI_I2S IT asserting rate is not the audio sampling rate.

The IT asserting rate seems to be totally de-correlated with the rate of reception of a sample from the microphone.Has somebody already used a microphone MEMS I2S ICS-43434 by InvenSense-TDK ?I don't succeed to connect a stereo pair of this microphon...

STM32G030F6 I2C2 set to slave mode, it can not work fine.

I am newer in STM32G030 develop.I tried to set STM32G030F6 I2C2 slave mode with PC.Q1.Using "HAL_I2C_Slave_Transmit(); it seems Master (PC) read 8 bytes later and stop. The other data will not read.Q2. If used HAL_I2C_Slave_Transmit_IT(), It only wr...

RSun.1 by Associate
  • 749 Views
  • 0 replies
  • 0 kudos

Can't figure out why RTC wakeup event doesn't work

Hello,I've followed all the steps required to generate and handle a RTC wakeup in the manual, but it still doesn't work. I can't figure out why that doesn't work.The goal of the following code is that, when I click the reset button of my nucleo L152-...

BCora.1 by Associate III
  • 2177 Views
  • 5 replies
  • 0 kudos

Resolved! STM32L412KB clock options

Im using a STM32L412KB for the first time and Im a little confused about the clock options. I can't seem to change the clock speed (input frequency) in cubeIDE, it's always stuck on 8MHz. However I notice there is an internal oscillator - does this m...

deep_rune by Associate III
  • 1045 Views
  • 3 replies
  • 0 kudos