STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H743 ADC Conversion/Sampling time

Hi,I wonder if the STM32H743 can sample and convert 1 ADC sample in 10 nanoseconds?According to the specs the ADC speed (sample + convert) at 14bit resolution with 50MHz ADC clock , one sample will take 200 nanoseconds.I have no problem lowering the ...

deckhard by Associate III
  • 1808 Views
  • 5 replies
  • 0 kudos

Callback take long time to trigger

MCU STM32L431, SYSCLK 80MHzThe callback takes 1.5us to fire from pin drop, and the callback functions take long time to execute as I show the imagethe pin config function/** * @brief GPIO Initialization Function * @param None * @retval None */static ...

JSanz.1 by Associate III
  • 2798 Views
  • 5 replies
  • 0 kudos

Resolved! RM0440, Rev 4, STM32G4 Reference Manual - typos

Table 226 on page 906 has an entry HRTIM_TIMxCMP1CR <- I don't think this is a real register.Section 27.3.8, page 888 second line in last paragraph says "any of the 5 timers". I think that should be 6 timers.Section 27.5.66, page 1050 says Bits 31:0 ...

HALL bug not setting clock ?

Hello. I was working on example generated by cubeMX (new version) on STM32L562VET6Q processor and canbus.Example code of networking worked just fine, but copying code to my LL based project made CANBUS inoperable.I was able to track down what is diff...

Linas L by Senior II
  • 1153 Views
  • 1 replies
  • 0 kudos

STM32L0x2 bug in reference manual

RM0376 Reference manual for STM32L0x2 DocID025941 Rev 5 states in 14.9 "Temperature sensor and internal reference voltage" :The following formula gives the actual VDDA voltage supplying the device: VDDA = 3 V x VREFINT_CAL / VREFINT_DATAThis can't be...

MWebj by Associate III
  • 3243 Views
  • 6 replies
  • 0 kudos

Pipeline stage explanation

hi, all. I wanted to ask about The pipeline stages in the m cortex processors , i read that m0 has 3 stages and m0+ has 2 , which renders it more efficient , can anyone explain what that means?

AMat.1 by Associate II
  • 1824 Views
  • 1 replies
  • 0 kudos

F7 UARTs Anything special?

The F4 board worked fine doing UART DMA. I start to regret this upgrade.Forget DMA and IT for now, just trying to get F7 polling working.First HAL_UART_Receive works, but the rest time out.Register analysis is unenlightening going by RM0385 referen...

Sking.21 by Associate III
  • 1798 Views
  • 3 replies
  • 0 kudos