STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! For STM32H745XI-Disco board are there example source code for initializing and using CRC , SDRAM and also using the EMMC 4GB flash .

Hi ,We need to develop driver for 4GB EMMC flash and SDRAM .For STM32H745XI-Disco board is there example source code for initializing and using CRC , SDRAM and also using the EMMC 4GB flash .Thanks In Advance

STM32L412: When I turn the reset (physical) switch, the µC jumps into the DFU bootloader, although it isn't supposed to

Hi there!I have a weird problem, where I'm a bit lost, probably also due to my limited knowledge of assembly. So I am trying to write a function (which is called using a very secret pattern) which sets a magic number and soft resets the microcontroll...

SPI Communication with STM32G031 using HAL

Hello,I tried to configure the STM32G031K8 Nucleo Board using CubeMX to send a request to an attached sensor using SPI1. To my request (2 bytes) the sensor should answer with 4 bytes. I configured the data size to 8 bits and the clock parameters core...

CLau.1 by Associate
  • 1198 Views
  • 0 replies
  • 0 kudos

Resolved! How to use HAL i2c and math.h in same project?

Hi everyone! I am using STM32F4 and IMU to read gyro and accelerometer, and than calculate IMU's euler angles. I can get data from IMU it is OK but when I try to add something from math.h program stops working but it also don't gives error or warninn...

0693W000004JjWRQA0.png 0693W000004JjZ5QAK.png
MDoğr.1 by Associate II
  • 1544 Views
  • 1 replies
  • 0 kudos

timer

I am using NUCLEO-H743ZI2. I am trying timer to generate pulse using TIM_OCMODE_TOGGLE channel 1. my timer clock is 100MHz, I set pre-scaler as 9 and channel 1 pulse as 9 as well. It seems it is difficult to get pulse, except I add more count on chan...

yang hong by Associate III
  • 849 Views
  • 3 replies
  • 0 kudos