STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Cortex M4 upgrade with STMG0 QFN32/48 pinout

Hi, thank you very much for the STM32G0 series, this really is very nice.Just for some applications I would need optioinally more CPU power, esepecially divide and best also floating point (so Cortex M3/M4 woudl be nice).I do NOT need higher speed / ...

flyer31 by Senior
  • 1800 Views
  • 2 replies
  • 0 kudos

Resolved! How to send and recevie data from serial print.

I'm using servo and driving it with servo motor. I want to print the servo degree via UART to serial. But im getting unknown characters. My code is;/* USER CODE BEGIN 0 */ uint32_t potadc; uint32_t servopot; /* USER CODE END 0 */   /* USER CODE BEGI...

sangarius by Associate II
  • 5519 Views
  • 21 replies
  • 0 kudos

Hi, I am new to this, and I just bought the P-NUCLEO-IOM01M1 master board , and I am trying to follow the UM2421-guide and trying to setup a connection to another device (TA2212, from Ifm), but the connection cant be established.

The control tool can correctly identify the Imported IODD-file, but when i try to setup the IO-link communication in the control-tool I recieve the COMLOST fault. Furthermore I receive an Event error with the code: 49415. The STEVAL-IOM001V1 is corre...

0693W0000059iviQAA.png
FAger.1 by Associate II
  • 726 Views
  • 0 replies
  • 0 kudos

Resolved! Bricked After first Debug STM32H735G-DK

I bought this kit to learn but after first time debugging i can't connect to it at all.I just set some GPIO input and outputs and got a led working in debug mode and now i can't connect to the board again and the previous debug program doesn't work e...

talan.1 by Associate
  • 2845 Views
  • 3 replies
  • 0 kudos

Resolved! Configuring LPTIM to generate autoreload interrupts on STM32L4

Hi,I am trying to learn how to use the LPTIM1 of the STM32L433 Nucleo-64 board (with the CPU: STM32L433RCTxP). I want to experiment on generating an interrupt every second with the LPTIM (I usually use a TIMx peripheral for this, but was interested b...

RrW1 by Associate III
  • 5814 Views
  • 4 replies
  • 0 kudos

Resolved! HAL_SPI_Transmit does not work.

Hello everyone,I try to transmitt data with my STM32L4A6ZG via SPI. I configured the Transmitt Only MasterMode and have NSS via hardware selected. After Initialization I check with the function: ret_tx1 = HAL_SPI_GetState(&hspi1);Which returns: HAL_S...

SWink by Associate II
  • 2908 Views
  • 2 replies
  • 0 kudos

Resolved! QSPI 32 bit addressing mode in STM32H753XI

I'm using STM32H753XI Eval 2 board with MT25QL01GBBB external flash on QSPI interface.I've configured it in 4 byte addressing mode but I'm not able to read the data correctly.I've referred code from here,https://github.com/STMicroelectronics/STM32Cu...

AShel.1 by Associate III
  • 3459 Views
  • 6 replies
  • 0 kudos

Resolved! STM32H743 ADC single-end and differential input configuration

Hi,I use ADC1_INP2 for single-end mode , how the ADC1_INN2 connect to?Internal VREF- or outside GND? And in differential mode,ADC1_INP6/ADC1_INN2 use de same pin, is that i can only use ADC1 channel 2 in differential mode? ADC1 channel 6 can't be use...

lsong.1 by Associate II
  • 2017 Views
  • 1 replies
  • 0 kudos