STM32H750 GPIO slow compared to STM32F2 series
Driving a RGB led matrix display (HUB75E) using custom board made with STM32H750. Earlier the prototype was made with STM32F205 and there was a minute flickering in some scenarios (brightness low). so thought of designing the board with STM32H7. But in STM32H7 the flickering is higher than STM32F2 (way higher). No other processing is happening in this testing.
what is the maximum GPIO switching frequency in STM32H7? does H7 series have any drawback in GPIO performance (even though it have the highest cpu clock)
CPU is clocked with HSE 480MHz (25MHz external crystal)