STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H7RS SPI DMA memory to/from peripheral

Hi,I am trying to establish a successful transfer using SPI in master full duplex DMA mode using a NUCLEO-H7S3L8 board (STM32H7RSxx family)..The runs and SPI data can be seen from the MOSI pins, but with one problem: data is not successfully sent.In ...

simozz_0-1749735236467.jpeg
simo zz by Senior II
  • 2270 Views
  • 9 replies
  • 2 kudos

Resolved! How to connect SMPS when it is not used in STM32U545?

I'm designing a custom PCB with STM32U545NEY6Q and I don't need to use the SMPS, only the LDO. I'm not sure how to connect the SMPS, I found a post about the STM32H745IIT6, and followed the same procedure, but should I do that? I followed the datashe...

Screenshot from 2025-06-17 11-21-57.png
leo8 by Associate
  • 1179 Views
  • 1 replies
  • 0 kudos

Resolved! STM32 Stop FMC Request

I've setup the FMC peripheral of an STM32H7 to read registers from an FPGA by creating a faux SRAM interface on the FPGA.  This works just fine so long as the FPGA has no issues but if, say, the FPGA is unprogrammed or the FPGA data bus gets hung, th...

Resolved! STM32F407 VDDA-VREF+ difference

In the STM32F407 DS, ADC characteristics table has the following footnotes:IMO 2. follows from 3. (which is a more stringent requirement); thus 2. is redundant and confusing.JW

waclawekjan_0-1749462029823.png

Custom STM32L476 based board LSE and HSE

Hello everyone, so it is my first time designing a board with stm32l476rg MCU. I was using the reference design from this sheet: https://www.st.com/resource/en/application_note/an4555-getting-started-with-stm32l4-series-and-stm32l4-series-hardware-de...

Stm325_0-1750208146036.png Stm325_1-1750208251627.png
Stm325 by Associate III
  • 920 Views
  • 2 replies
  • 0 kudos

Resolved! Simultaneous dual mode adc not working for me

Hi, I'm using the STM32H7 family and have spent several days trying to get dual mode working correctly with the STM32H723.  I finally switched to the STM32H753 so I could try the ADC_DualModeInterleaved example from the repository at STM32CubeH7/Proj...

EMarq.1 by Associate II
  • 826 Views
  • 1 replies
  • 0 kudos

STM32H735 with Ethernet & LAN8710A PHY

Hello I am triyng to use STM32H735 with ethernet (ln8710A is the PHY) We have hardware fault when we connect the cable (se the itm print below)We use CubeMx version Version: 1.18.0ETH is in RMII conection is OK      

dacha1_1-1750063232727.png dacha1_2-1750063273389.png dacha1_0-1750062122111.png
dacha.1 by Associate II
  • 1983 Views
  • 7 replies
  • 0 kudos