STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Manipulating MCU SPI Interface to Access a Nonstandard SPI

HI There,I want to access multiple SPI slaves at the same time.They all share the same CLK , the same MOSI pin and the same CS.Therefore, I wrote two code sections which basically should do the same.They kind of work, but they both have the same Prob...

TOne.1 by Associate II
  • 2704 Views
  • 8 replies
  • 0 kudos

USART in interrupt mode

Hi, I want to use USART in interrupt mode in stm32f429 evaluation board.I saw the demo example UART_Hyperterminal_IT, but I didn't understood why they are calling HAL_UART_Receive_IT() function if we are using USART in interrupt mode not in polling m...

PNaph.2 by Associate II
  • 1091 Views
  • 2 replies
  • 0 kudos

STM32F103RGT6 I2C state machine misunderstanding

Hello.I'm trying to get I2C working to read BMP280 sensor data. This is code I written so far: GPIOB->CRL |= GPIO_CRL_MODE6; //set PB6 as output with drive strenght to 50Mhz GPIOB->CRL |= GPIO_CRL_CNF6; //set PB6 to open-drain alternate funct...

fifi_22 by Associate III
  • 944 Views
  • 0 replies
  • 0 kudos

What is the recommended Software Test Tool that conforms to White Box Testing for STM32? I have a finished project code in STM32CubeIDE but it has to pass the FDA Software Test (independent of hardware).

This link provides details regarding White Box Testing: https://www.softwaretestinghelp.com/white-box-testing-techniques-with-example/Basically we just want to test the software by conducting a white box unit test. Any input is much appreciated. Than...

KGayo by Associate
  • 854 Views
  • 0 replies
  • 0 kudos

Bug when erasing flash STM32F412

Hello. Errata writes interesting things.2.1.7 Flash sector erase issue for sectors 5 to 11DescriptionUnder specific conditions, flash erase issues are observed.The involved sectors are: 5 to 11WorkaroundDo not perform sector erase on sectors 5 to 11....

Arlleex1 by Associate III
  • 4550 Views
  • 9 replies
  • 0 kudos

Stlink deleteded inside firmware

Hello thereI am currently working with the stm32f7469-disco card, I accidentally deleted the software inside the st link, I wonder how do I restore it?

ÖDemi.1 by Associate II
  • 1083 Views
  • 1 replies
  • 0 kudos