cancel
Showing results for 
Search instead for 
Did you mean: 

Is it a problem if the NJTRST pin is toggled before it is disabled and configured as GPIO (JTAG is not needed)?

ChristophR
Associate III

Hi,

I have a design with a STM32F301 controller. I don't need JTAG, therefore I want to reuse the JTAG pins for other purposes.

Is it a problem if the NJTRST signal is toggled when the uC is starting up? Could this affect the uC operation, or does this just reset the JTAG logic without affecting the core?

As soon as the application is running, the JTAG port is disabled.

Thanks!

Best regards, 

Christoph

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
waclawek.jan
Super User

>Could this affect the uC operation, or does this just reset the JTAG logic without affecting the core?

IMO the latter.

JW