2020-07-08 4:29 AM
Hi,
AN2606 (STM32 microcontroller system memory boot mode) states e.g. for the STM32F301, that in system memory boot mode both USART_TX pins (USART1_TX & USART2_TX) are used as outputs.
Is the TX pins really configured as outputs as soon as the system memory mode is entered, or are the pins only configured as outputs as soon as the UART frame 0x7F for bootloader selection is received on the USART_RX pin?
Thanks!
Best regards,
Christoph
2020-07-08 4:01 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.