Interrupts Management
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-07-07 6:46 AM
I am trying to understand the priorities, subpriorities and priority grouping in my stm32f407-Discovery.
I would like to have 3 external LEDS (LD_A, LD_B, LD_C) and 3 interrupts (IT_A, IT_B, IT_C) with. IT_A has a highest priority, IT_C has the lowest one.
IT_A turns off LD_B and LD_C but turns on LD_A. The other interrupts work accordingly.
What I want:
When the IT_B happens, the IT_C should not happen but the IT_A should happen.
What I get:
No matter what interrupt happens first it seems that it steals the whole cycles of the CPU and the other interrupts cannot happen.
Here is the source code:
...
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
#define STATE_SIZE 3
#define COUNTER_SIZE 4
/* USER CODE END PD */
/* USER CODE BEGIN PV */
uint8_t state[STATE_SIZE] = {RESET, RESET, RESET};
uint8_t counter[COUNTER_SIZE] = {0, 0, 0, 0};
uint8_t firstRun = 1, red = 0, blue = 0;
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
HAL_NVIC_SetPriorityGrouping(NVIC_PRIORITYGROUP_1);
while (1)
{
if (firstRun) {
firstRun = 0;
HAL_GPIO_WritePin(Red_External_LED_GPIO_Port, Red_External_LED_Pin, RESET);
HAL_GPIO_WritePin(Blue_External_LED_GPIO_Port, Blue_External_LED_Pin, RESET);
HAL_GPIO_WritePin(Green_External_LED_GPIO_Port, Green_External_LED_Pin, RESET);
HAL_Delay(500);
HAL_GPIO_WritePin(Red_External_LED_GPIO_Port, Red_External_LED_Pin, SET);
HAL_Delay(500);
HAL_GPIO_WritePin(Blue_External_LED_GPIO_Port, Blue_External_LED_Pin, SET);
HAL_Delay(500);
HAL_GPIO_WritePin(Green_External_LED_GPIO_Port, Green_External_LED_Pin, SET);
HAL_Delay(500);
HAL_GPIO_WritePin(Green_External_LED_GPIO_Port, Green_External_LED_Pin, RESET);
HAL_Delay(500);
HAL_GPIO_WritePin(Blue_External_LED_GPIO_Port, Blue_External_LED_Pin, RESET);
HAL_Delay(500);
HAL_GPIO_WritePin(Red_External_LED_GPIO_Port, Red_External_LED_Pin, RESET);
HAL_Delay(500);
}
}
}
/**
* @brief GPIO Initialization Function
* @param None
* @retval None
*/
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOE_CLK_ENABLE();
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOH_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
__HAL_RCC_GPIOD_CLK_ENABLE();
/*Configure GPIO pins : Green_External_LED_IT_Pin Red_External_LED_IT_Pin Blue_External_LED_IT_Pin */
GPIO_InitStruct.Pin = Green_External_LED_IT_Pin|Red_External_LED_IT_Pin|Blue_External_LED_IT_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING_FALLING;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);
/* EXTI interrupt init*/
HAL_NVIC_SetPriority(EXTI0_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(EXTI0_IRQn);
HAL_NVIC_SetPriority(EXTI1_IRQn, 0, 1);
HAL_NVIC_EnableIRQ(EXTI1_IRQn);
HAL_NVIC_SetPriority(EXTI2_IRQn, 1, 1);
HAL_NVIC_EnableIRQ(EXTI2_IRQn);
}
/* USER CODE BEGIN 4 */
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
if (GPIO_Pin == Red_External_LED_IT_Pin) {
state[0] = HAL_GPIO_ReadPin(Red_External_LED_IT_GPIO_Port, Red_External_LED_IT_Pin);
counter[0]++;
blue = 0, red = 1;
while(red) {
HAL_GPIO_TogglePin(Red_External_LED_GPIO_Port, Red_External_LED_Pin);
for(int i = 0; i < 1000000; i++);
}
}
else if (GPIO_Pin == Blue_External_LED_IT_Pin) {
state[1] = HAL_GPIO_ReadPin(Blue_External_LED_IT_GPIO_Port, Blue_External_LED_IT_Pin);
counter[1]++;
red = 0, blue = 1;
while(blue) {
HAL_GPIO_TogglePin(Blue_External_LED_GPIO_Port, Blue_External_LED_Pin);
for(int i = 0; i < 1000000; i++);
}
}
else if (GPIO_Pin == Green_External_LED_IT_Pin) {
state[2] = HAL_GPIO_ReadPin(Green_External_LED_IT_GPIO_Port, Green_External_LED_IT_Pin);
HAL_GPIO_WritePin(Green_External_LED_GPIO_Port, Green_External_LED_Pin, state[2]);
counter[2]++;
}
else {
counter[3]++;
}
}
- Labels:
-
Interrupt
-
STM32F4 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-07-08 3:26 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-07-08 12:57 PM
You should've gathered this information from the Programming Manual to the processor core of your STM32 model (i.e. Cortex-M4).
JW