STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H7 (dual core) ADC1/2/3 ressource split

Hello,I have one question regarding the ADC1/2/3 cores for the STM32H7 (dual core solution). Let's say, I would like to split few ADC channels between both ADC cores and Cortex cores. Is it possible to assin channels 1,2,3 for ADC1 core (regular grou...

PButc.1 by Associate II
  • 1172 Views
  • 1 replies
  • 0 kudos

Unnecessary hardfault due to button press on system wakeup pin.

We are trying to build a USB Data Logger We are facing some issue while being in run mode. Initially system is in standby mode and can be woken using button press (connected to system wakeup 1). On 5 sec press system/mcu starts logging data into flas...

JKSah by Associate II
  • 2905 Views
  • 6 replies
  • 0 kudos

PWM Timer and GPIO level

Hello,I'm using a STM32F091 with TIM2 configured in PWM mode.(and CH1-CH2 connected to an output)After some hundreads of milliseconds, I have to stop the PWM by setting CCRx at 0. And reenable later.So far so good.But to improve my working, I would t...

PCu1 by Senior
  • 2492 Views
  • 5 replies
  • 0 kudos

Can't access STM32L552 after setting SRAM2-RST to 0

I've been trying to run the SBSFU example from STM32Cube_FW_L5_V1.2.0.The option bytes I set initially were:TZEN=1DBANK=1 (was already 1)SECWM1_PSTRT=0x0 and SECWM1_PEND=0x7fSECWM2_PSTRT=0x1 and SECWM2_PEND=0x0.That allowed me to load SBSFU bootloade...

tosa by Associate
  • 1669 Views
  • 2 replies
  • 0 kudos

Typo in several documents (wait sates)

I came across "wait sates" (with missing "t") in RM0316 rev.8, but just for the laugh I threw it into google (https://www.google.com/search?q="wait+sates"+site%3Ast.com ), and... lo and behold, this appears to be a quite often repeated typo, at least...

Resolved! Max current possibly sourced from a DAC pin?

Hello. I would like to know how much current a DAC pin is able to source. The STM32G081 datasheet indicates "Output current sourced by any I/O and control pin = 15mA". Is this 15mA also an upper limit to a DAC sourcing pin? The STM32G081 datasheet al...

JLemi by Associate III
  • 3632 Views
  • 3 replies
  • 0 kudos

Resolved! TIM2 freeze on ARR register value changed STM32H743ZI2

Hi. I'm working on project where I need short pulses with precise periods generated in audio ranges (10 - 20kHz). So I decided to choose TIM2 and using it in PWM mode. I'm using HAL library and configuration code generated by CubeMX:void MX_TIM2_Init...