STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Stm32f407 discovery board real or fake?

I have bought new STM32F407 DISCOVERY BOARD and I got blue board STM32F407 Discovery board so is it real or fake, while connecting via mini B cable also memory showing only approx. 20-30kb of space in it so please confirm it as real or fake?

SVerm.3 by Associate III
  • 2272 Views
  • 6 replies
  • 0 kudos

Resolved! All 0x00 in STM32G4 flash? Is it can be recover?

I am testing STLINK Utility's Automatic Mode for mass-production,I set read out protection in option byte from level0 to level1(I have never set it to level2,for its irreversibility),so I just plug in and out the STLINK acting as the operation of mas...

0693W000006ICNgQAO.png 0693W000006ICNlQAO.png 0693W000006ICM0QAO.png 0693W000006ICOyQAO.png
ZYu.1 by Associate III
  • 2950 Views
  • 3 replies
  • 0 kudos

Resolved! How to read Timer Capture triggered by software

I have an application where I am using an external signal to trigger TIM8_CH1 to do a capture and generate a DMA interrupt where I then store the counter value. I want to perform a similar action on an internal firmware (FW) signal. I want to store t...

BTrem.1 by Senior II
  • 1904 Views
  • 3 replies
  • 0 kudos

When will STM32G0x0 be available?

Everywhere I check online, I cannot find any STM32G070 chips. I'm looking to up my game from 8-bit AVR to 32 ARM MCUs that stay in the same price range.

EFrei.2 by Associate
  • 1036 Views
  • 1 replies
  • 0 kudos

Which parts of an .ELF file go into the .bin file?

(since I am getting "Error while parsing Rich Text Content" in the saved post all the time, even though in the EDITOR everything renders just fine, I dumped the text in there without nice formatting)---------------------------------------------------...

SKled.1 by Senior II
  • 5534 Views
  • 5 replies
  • 0 kudos

Mount problems with SD Card greater than 1G

Dear all,i'm developing an application with STM32F750N8 and I'm using SDMMC peripheral (48MHz clock, rising clock transition, no prescaler and hardware flow control) and FatFs library, for read and write the micro SD Card.I tried to use a 1GB SD Card...

Luca G. by Associate III
  • 3974 Views
  • 5 replies
  • 0 kudos