STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Max current possibly sourced from a DAC pin?

Hello. I would like to know how much current a DAC pin is able to source. The STM32G081 datasheet indicates "Output current sourced by any I/O and control pin = 15mA". Is this 15mA also an upper limit to a DAC sourcing pin? The STM32G081 datasheet al...

JLemi by Associate III
  • 3558 Views
  • 3 replies
  • 0 kudos

Resolved! TIM2 freeze on ARR register value changed STM32H743ZI2

Hi. I'm working on project where I need short pulses with precise periods generated in audio ranges (10 - 20kHz). So I decided to choose TIM2 and using it in PWM mode. I'm using HAL library and configuration code generated by CubeMX:void MX_TIM2_Init...

Stm32f407 discovery board real or fake?

I have bought new STM32F407 DISCOVERY BOARD and I got blue board STM32F407 Discovery board so is it real or fake, while connecting via mini B cable also memory showing only approx. 20-30kb of space in it so please confirm it as real or fake?

SVerm.3 by Associate III
  • 2131 Views
  • 6 replies
  • 0 kudos

Resolved! All 0x00 in STM32G4 flash? Is it can be recover?

I am testing STLINK Utility's Automatic Mode for mass-production,I set read out protection in option byte from level0 to level1(I have never set it to level2,for its irreversibility),so I just plug in and out the STLINK acting as the operation of mas...

0693W000006ICNgQAO.png 0693W000006ICNlQAO.png 0693W000006ICM0QAO.png 0693W000006ICOyQAO.png
ZYu.1 by Associate III
  • 2847 Views
  • 3 replies
  • 0 kudos

Resolved! How to read Timer Capture triggered by software

I have an application where I am using an external signal to trigger TIM8_CH1 to do a capture and generate a DMA interrupt where I then store the counter value. I want to perform a similar action on an internal firmware (FW) signal. I want to store t...

BTrem.1 by Senior II
  • 1812 Views
  • 3 replies
  • 0 kudos

When will STM32G0x0 be available?

Everywhere I check online, I cannot find any STM32G070 chips. I'm looking to up my game from 8-bit AVR to 32 ARM MCUs that stay in the same price range.

EFrei.2 by Associate
  • 990 Views
  • 1 replies
  • 0 kudos