2020-09-24 11:13 AM
Hi
Iam using CUBEMX and kiel for my development. iam read date time from the GSM modem
when i read it from the modem its looks like this.
+QLTS: "20/09/24,18:08:18+22,0"+22 mean my time zone(+5:30). my actual time at this time is
2020:09:24 23:38:20
i will extract year, month..... from the above string and pass it into another function
void update_Internal_RTC(Time_t set_time){
RTC_TimeTypeDef set_Time = {0};
RTC_DateTypeDef set_Date = {0};
set_Time.Hours = set_time.Hour;
set_Time.Minutes = set_time.Minute;
set_Time.Seconds = set_time.Second;
if (HAL_RTC_SetTime(&hrtc, &set_Time, RTC_FORMAT_BIN) != HAL_OK)
{
Error_Handler();
}
set_Date.Month = time.Month;
set_Date.Date = time.Date;
set_Date.Year = time.Year;
printf("year is %d\r\n",time.Year);
if (HAL_RTC_SetDate(&hrtc, &set_Date, RTC_FORMAT_BIN) != HAL_OK)
{
Error_Handler();
}
}now i want to add my time offset before sent it to RTC module. simply i need add 19800 (5:30) seconds before save it on the timer. what is the simplest way
Greetings
2020-09-24 11:30 AM
The simplest way is to convert the time to seconds in some epoch, add seconds, and convert time back. Use the standard C library functions prototyped in <time.h>.
JW
2020-09-24 12:03 PM
Decide what time you want to use in your system, and then stick with it, and do conversions as necessary.
Personally, I'd stick with ZULU time (GMT/UTC), and remember the current time zone, I live in a country spanning multiple zones.
When I need a LOCAL time stamp, I'd convert into that, and use that to generate TIME and DATE
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.